Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    SMPS Design Secrets: Master DCM and CCM Modes Today

    Power supplies are the unsung heroes of electronic devices, ensuring precise, stable DC voltages reach your circuits. But the magic behind these workhorses...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
ADSP-BF70x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF70x
  • Processors & DSP
  • Blackfin Processors
  • ADSP-BF70x
  • Cancel
ADSP-BF70x
Documents Hardware Reset using Watchdog in BF706
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • -ADSP BF706 FAQ:
    • Hardware Reset using Watchdog in BF706
    • ADSP BF706 Ezkit Mini SPI1 cannot be done in master mode.
  • +ADSP-BF707: FAQ
  • +ADSP-BF70X: FAQ

Hardware Reset using Watchdog in BF706

The attached example code that illustrates how to configure the interrupt coming from Watchdog as “FAULT” in the SEC and that resets the processor.  This code can be directly run on the ADSP-BF706 EZ-Kit MINI.

In order to demonstrate this scenario, the LED0 in the EZ-kit MINI is turned ON in the application code and watchdog timer configured to issue a reset via the SEC Fault Interface (SFI). Watchdog count never reloaded and hence it expires according to the count value given and that issues system reset upon expiry through Fault Management Unit (FMU). When you boot this application you would see that LED0 turns ON for a while and it goes off because of watchdog expiration that reset the processor. After processor reset it boots again and this loop continues.WDG_HWReset_706.zip

Tags: Audio Signal Processors Blackfin Embedded Processors adsp-bf706