Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
ADSP-BF70x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF70x
  • Processors & DSP
  • Blackfin Processors
  • ADSP-BF70x
  • Cancel
ADSP-BF70x
Documents Example for UART transmit and receive operation using Core Mode for BF707
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP BF706 FAQ:
  • -ADSP-BF707: FAQ
    • Example for UART transmit and receive operation using Core Mode for BF707
    • ADSP-BF707 - DDR Memory Test
    • ADSP-BF707 Preserve data after RESET
    • What Secure Boot Modes are supported in ADSP-BF707?
    • GPIO example code for BF707
    • SPI example in Autobuffer mode on BF707
    • BF707 SPI Slave to Master loopback communication
    • Code Example: SPI Memory-Mapped mode
  • +ADSP-BF70X: FAQ

Example for UART transmit and receive operation using Core Mode for BF707

Please refer the attached example for UART transmit and receive operation using Core Mode.  An external connection is required to connect UART0 and UART1 pins.

Connect pin PB-08(UART0 TX) and PC-01(UART1 RX) pin.BF707_UART_Int.zip