Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain

    In this webinar, we will reassess the design of electronics for Flow Cytometry applications. In the past, 20-bit, 40 MSPS analog-to-digital converters...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
ADSP-BF70x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF70x
  • Processors & DSP
  • Blackfin Processors
  • ADSP-BF70x
  • Cancel
ADSP-BF70x
Documents the secret BF70x documentation
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP BF706 FAQ:
  • +ADSP-BF707: FAQ
  • -ADSP-BF70X: FAQ
    • Different Wake-up Sources on BF70x
    • ADSP-BF70x application cannot boot using Secure Boot
    • CPLB enhancements in Blackfin+ Core
    • FAQ: Different Wake-up Sources on BF70x
    • Digital watch code for RTC
    • Enhancements in Hardware Loop in Blackfin+ core
    • Enhancements in Supervisor Mode in Blackfin+ core
    • HADC maximum bandwidth
    • Highlights of MSI on BF70x
    • How can I initialize DDR memory device connected to BF70x processor ?
    • How do I access the full memory space of the SPI slave?
    • How L2CTL in BF70x is different than BF60x ?
    • How the System Cross Bar (SCB) in BF70x different than in BF60x ?
    • How to configure MSI IDMAC for Dual Buffer Descriptor Ring mode operation
    • FAQ: How to re-enable the Core clock on BF70x after gating it
    • How to send data using SPI READY signal
    • How to take the core out of reset on BF70x
    • How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)
    • Is INIT Code supported in Secure Boot in ADSP-BF707
    • Monitoring Cache Performance on the ADSP-BF70x
    • Performance Enhancements in Blackfin+ core
    • UART slave boot BF70x with Higher BAUD rate
    • Sample code for HADC on BF70x?
    • What are the salient features of SPI Host Port on BF70x?
    • What is the effect of bus disabling (RDEN bit) on RTC functionality?
    • What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module
    • What is the purpose of the ownership bit when programming the PKTE module for encryption/hashing?
    • What modes of Encryption and Hashing are supported and how do they make an application secure
    • Getting Started with ADSP-BF70x Processors
    • How to re-enable the Core clock on BF70x after gating it
    • Known Errata Against ADSP-BF70x Blackfin+ Datasheet
    • the secret BF70x documentation
    • Where can I find power consumption data for BF70x processors?
    • What are the major differences between DMC module of BF60x and BF70x ?
    • Cache Enhancements in Blackfin+ core
    • Can I pass the output generated from PKA directly to the PKTE module for encryption/decryption
    • Configuring Timer in continuous/single pulse mode
    • ADSP-BF70X BLACKFIN PROCESSOR SUPPORT COMMUNITY
    • DMA error interrupt
    • How to verify that the boot bytes are accurate in all boot modes for the ADSP-BF60x and ADSP-BF70x?

the secret BF70x documentation

For anyone trying to evaluate the BF70x for design-in, there are definite gaps in the documentations.

I don't claim to have all the answers, but I'm posting what I've managed to infer in the hopes that it saves someone else some anguish.


RE: the secret BF70x documentation by pinaz:

Lesson 1:

Figure 36-8 in the Hardware Reference Manual (Revision 0.2, May 2014) is inaccurate/incomplete. Refer to the "BITM_ROM_BCMD_" #define values in "defBF70x_rom.h" in the CrossCore IDE.


RE: the secret BF70x documentation by pinaz:

Lesson 2:

An essential piece of information not found in any Analog document is the following table that should accompany a corrected version of Figure 36-8:

NOAUTO BCODE DUMMY ADDR SPEED
0 ignored ignored ignored ignored
1 used used used used

In other words, when NOAUTO is not set, the BCODE, DUMMY, ADDR, and SPEED values are ignored.


RE: the secret BF70x documentation by pinaz:

Lesson 3:

Table 36-14 in the Hardware Reference Manual and the preceding text implies that selection of "SPIMCODE" (called "BCODE" in "defBF70x_rom.h") controls the Command, Dummy Bytes, and SPI Clock.  However, this is not true.

SPIMCODE / BCODE appears to only control which command byte is used.


RE: the secret BF70x documentation by pinaz:

Lesson 4:

Table 36-14 in the Hardware Reference Manual doesn't enumerate what the algorithms and/or assumptions are in booting.

For example, both SPIMCODE / BCODE modes 0xA " QOR FAST_MODE (Atmel) " and 0xC " QOR FAST_MODE " appear to boot the Winbond W25Q32 populated on the ADZS-BF707-EZBRD.

However, mode 0xC is at a considerable performance disadvantage to mode 0xA.

For an unexplained reason, mode 0xC wastes 11-12 milliseconds continuously polling with a RDSR (Read Status Register 05h) command, which costs that much in extra boot time.

Mode 0xA also issues a RDSR, but only does so for four SPI cycles.  It doesn't seem the polling is waiting for a change of value; it just issues that number of transactions.


RE: the secret BF70x documentation by pinaz:

Here is some collected data on the SPI clock speed in different boot modes using BF707 0.0 silicon on a ADZS-BF707-EZBRD development board.  As you will see, some boot modes appear to be broken.

BootCMD BCODE SPEED measured SPI clock MHz
F0210242 1 F 6.25
80210242 1 8 11.11
F0220242 2 F 6.25
80220242 2 8 11.11
F0230242 3 F 6.25
80230242 3 8 11.11
F0640242 4 F 6.25
80640242 4 8 11.11
F0680242 8 F 6.25
80680242 8 8 11.11
F0690242 9 F 6.25
80690242 9 8 11.11
F06A0242 A F 3.125
806A0242 A 8 3.125
F06C0242 C F 3.125
806C0242 C 8 3.125

The "quad" SPI modes of BCODEs A and C ought to offer extra speed.  However, if the clock rate is stuck, it could erode the advantage and cost boot time.