Post Go back to editing

Is SCLK0 always limited to 50MHz when using the SMC?

Category: Datasheet/Specs
Product Number: ADSP-BF707

Hello,

I have a question regarding the static memory controller, and whether or not SCLK0 is always limited by CLKOUT when using it.

I know that the limits for SCLK0 and CLKOUT are 100MHz and 50MHz respectively, and the following statement can be found in the datasheet:

SMC Read Cycle Timing With Reference to SYS_CLKOUT
The following SMC specifications with respect to SYS_CLKOUT are given to accommodate the connection of the SMC to
programmable logic devices. These specifications assume that SYS_CLKOUT is outputting a buffered version of SCLK0 by
setting CGU_CLKOUTSEL.CLKOUTSEL = 0x3. However, SCLK0 must not run faster than the maximum fOCLK specification.

So it is clear that, when using the interface in a synchronous fashion with CLKOUT, SCLK0 will indeed be limited to 50MHz as well.

However, what if the connected memory is asynchronous and I don't actually need CLKOUT? Can I operate the SMC at 100MHz as long as I don't select SCLK0 as the source for CLKOUT?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.