Post Go back to editing

Minimum Voltage threshold on USB0_VUSB in BF707?

Thread Summary

The user inquired about the allowable VBUS voltage drop when using a long USB cable with the ADSP-BF707. The minimum VBUS voltage is 4.40V for low-power ports and 4.75V for high-power ports, according to the USB 2.0 Specification. A VUSB of 4.75V is acceptable for normal operation.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADSP-BF707

Hi,

While use ADSP-BF707 with long length USB Cable, USB0-VUSB is about 4V due to cable Vdrop.  

What is the allowable Vdrop? voltage threshold to work normally with some Vdrop?  I know that the spec is 5V, by the way 4.75V is ok? or should be 5V exactly?

Best Regards, 

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.