HI ADI's
My customer is trying to capture CIS (Pixel Plus POC030K) images using the BF706 CPU, but the following phenomenon occurs
1) MCLK:25MHz (generated by timer), PCLK:25MHz -> Y only, YUV422 images are all cut in half.
2) MCLK:25MHz (generated by timer), PCLK:12.5MHz -> Y only image is normal, but wave-like appearance occurs in YUV422 image.
The EPPI and DMA settings files are attached.
Set EPPI and DMA related settings in the imc_configure function and start capturing through the imc_capture function.
(1) Image cut in half

(2) Normal image

(3) Image that appears to be shaking like a wave

Please check that
Thank you