Post Go back to editing

Calcuate sha256sum in PKTE in Direct Host Mode

Category: Software
Product Number: BF-706
Software Version: cces 2.1

I am trying to calculate sha256sum of a buffer of lenght 1 byte using PKTE in Direct Host Mode.

Following is my code:

/*****************************************************************************
 * sha_256_hw.c
 *****************************************************************************/

#include <sys/platform.h>
#include "adi_initialize.h"
#include <blackfin.h>

/** 
 * If you want to use command program arguments, then place them in the following string. 
 */
char __argv_string[] = "";

uint8_t buffer[] ="R";
#define LEN	1
uint32_t resblk[8];

void run_sha256sum_test (void)
{
	uint32_t datatmp = 0,i,j;
	//step 1 : reset the pkte engine and release from reset
	*pREG_PKTE0_CFG = 3;
	*pREG_PKTE0_CFG = 0; // PKTE_CFG.MODE=0 i.e. Direct Host mode


	//step 2 & 3 : Set the ownership back to the packet engine & Set the PKTE_CTL_STAT.HASHFINAL
	*pREG_PKTE0_CTL_STAT = 0x11;

	//Step 4: set size of the input data in bytes in the PKTE_LEN.TOTLEN bit field
	//Step 5: Also set the PKTE_LEN.PEDONE bit = 0 and the PKTE_LEN.HSTRDY bit =1.
	//		  These bits must be the same as the PKTE_CTL_STAT.PERDY and
	//		  PKTE_CTL_STAT.HOSTRDY bits to guarantee ownership.
	*pREG_PKTE0_LEN = 0x00400001; //lenght of the input buffer is 1

	//Step 6: Set the PKTE_CDSC_CNT register=1 to trigger the packet engine to
	//start validating the command descriptor.
	*pREG_PKTE0_CDSC_CNT = 1; //Just one command discrptor



	///Step 7: For an SHA, set the PKTE_SA_CMD0.OPCD bit field =0b011 for hash
	//			operation and the PKTE_SA_CMD0.OPGRP bit field =0b00 for basic operation.
	//Step 8: for SHA-256, PKTE_SA_CMD0.HASH =0b0011
	//Step 9: For SHA-256, PKTE_SA_CMD0.DIGESTLEN =0b1000 (8 words)
	//Step 10: setting the PKTE_SA_CMD0.HASHSRC bit field =0b11,
	//the packet engine provides the correct initial constants depending on the SHA chosen
	*pREG_PKTE0_SA_CMD0 = 0x0c803f03;

	//Step 11: Set the PKTE_SA_CMD1.CPYDGST bit =1 and
	//PKTE_SA_CMD1.CPYPAD bit =1 to move the result to the output buffer
	//of the packet engine at the PKTE_DATAIO_BUF location.
	*pREG_PKTE0_SA_CMD1 =0x09;

	//Step 12: Write to the PKTE_SA_RDY register with any value to trigger the operation.
	*pREG_PKTE0_SA_RDY = 1;

	//Step 13: Start writing the input to the data buffer of the packet engine starting
	//at the PKTE_DATAIO_BUF location
//TODO: implement loop to feed the input in 32-bit multiples

	*pREG_PKTE0_DATAIO_BUF = buffer[0]<<24 ;//rest are dont care

	//Step 14: Write the PKTE_INBUF_CNT register with the length of the input
	//rounded up to the next multiple of 4. For	example,
	//if the input length is 30 bytes, set this register to 32.
	*pREG_PKTE0_INBUF_CNT = LEN + ((LEN & 0xf) && 1);


	for (i=0;i<0x5ffff;i++)
		asm("nop;");
	//TODO: poll the stat register

	for (i=0;i<8;i++)
		resblk[i] = *pREG_PKTE0_DATAIO_BUF;


}

int main(int argc, char *argv[])
{
	/**
	 * Initialize managed drivers and/or services that have been added to 
	 * the project.
	 * @return zero on success 
	 */
	adi_initComponents();
	
	/* Begin adding your custom code here */
	run_sha256sum_test();


	return 0;
}

The writes to PKTE_LEN in step 4 & 5 are not getting reflected into the *pREG_PKTE0_LEN.

What am I doing wrong here?

Edit: Please note the steps mentioned in the comments in the code are from the Harware Refence Manual for BF70x Page 577



Adding the source of the steps followed in the code, also Including the links for Harware Refence Manual
[edited by: RishavAmbasta at 10:34 AM (GMT -5) on 9 Nov 2023]
Parents Reply Children
No Data