Hi,
My customer would like to use external SRAM rather than an SDRAM?
Can DMC support SRAM?
Do we have any processor family that can support external SRAM?
Thx.
Mert
Hi,
My customer would like to use external SRAM rather than an SDRAM?
Can DMC support SRAM?
Do we have any processor family that can support external SRAM?
Thx.
Mert
Hi Mert,
The ADSP-BF70x processor supports SMC which can be connected to SRAM.
The static memory controller (SMC) is a protocol converter and data transfer interface between the internal processor bus and the external L3 memory. It provides a glueless interface to various external memories and peripheral devices, including:
• SRAM
• ROM
• EPROM
• NOR flash memory
• FPGA/ASIC devices
The SMC acts as an SCB target. The processor SCB interconnect fabric arbitrates accesses to the SMC. On the chip boundary, the SMC connects to an address bus, a data bus, and signal pins for memory control (such as read, write, output enable, and memory select lines)
For more information, please refer the chapter 10 Static Memory Controller (SMC) in the below link.
www.analog.com/.../BF70x_BlackfinProcessorHardwareReference.pdf
Regards,
Divya.P