Post Go back to editing

ADSP-BF706 SPI1 - DMA problem

I'm trying to make SPI1 via DMA work, but I don't see the signals on the oscilloscope, it doesn't work, it could help me. Here is the code:

boot:
void Init_SPI1(void)
{
/*
*pREG_SPI1_CLK = ( ( 9 << BITP_SPI_CLK_BAUD) & BITM_SPI_CLK_BAUD);

*pREG_SPI1_DLY = ( ((1 << BITP_SPI_DLY_STOP) & BITM_SPI_DLY_STOP) |
((1 << BITP_SPI_DLY_LEADX)& BITM_SPI_DLY_LEADX) |
((1 << BITP_SPI_DLY_LAGX) & BITM_SPI_DLY_LAGX) );

*pREG_SPI1_CTL = ( ((SPI1_MSTR << BITP_SPI_CTL_MSTR) & BITM_SPI_CTL_MSTR) |
((CPHA << BITP_SPI_CTL_CPHA) & BITM_SPI_CTL_CPHA ) |
((CPOL << BITP_SPI_CTL_CPOL) & BITM_SPI_CTL_CPOL ) |
((SPI_SIZE << BITP_SPI_CTL_SIZE) & BITM_SPI_CTL_SIZE ) |
((LSBF << BITP_SPI_CTL_LSBF) & BITM_SPI_CTL_LSBF ) |
BITM_SPI_CTL_ASSEL | BITM_SPI_CTL_SELST );


*pREG_SPI1_TXCTL = (ENUM_SPI_TXCTL_TWC_EN | ENUM_SPI_TXCTL_ZERO | ENUM_SPI_TXCTL_TDR_50 );

*pREG_SPI1_TWC = BUFF_SIZE;

*pREG_SPI1_TWCR = 0x00;

*pREG_SPI1_SLVSEL = (ENUM_SPI_SLVSEL_SSEL1_EN);
*/
*pREG_SPI1_CLK = 24;
*pREG_SPI1_DLY = 0; //((1 << BITP_SPI_DLY_STOP) & BITM_SPI_DLY_STOP) ;
*pREG_SPI1_SLVSEL= ENUM_SPI_SLVSEL_SSEL1_HI | ENUM_SPI_SLVSEL_SSEL1_EN;

*pREG_SPI1_CTL = ENUM_SPI_CTL_MASTER ;
*pREG_SPI1_TXCTL = ENUM_SPI_TXCTL_TTI_EN | ENUM_SPI_TXCTL_TWC_EN | ENUM_SPI_TXCTL_ZERO ;
*pREG_SPI1_RXCTL = ENUM_SPI_RXCTL_OVERWRITE ;

*pREG_SPI1_TXCTL |= ENUM_SPI_TXCTL_TX_EN; // enable Tx SPI
*pREG_SPI1_RXCTL |= ENUM_SPI_RXCTL_RX_EN; // enable Rx SPI
*pREG_SPI1_CTL |= ENUM_SPI_CTL_EN;
}

Pins Configuration:
#define UART0_TX_PORTB_MUX ((uint32_t) ((uint32_t) 0<<16))
#define UART0_RX_PORTB_MUX ((uint32_t) ((uint32_t) 0<<18))

#define UART0_TX_PORTB_FER ((uint32_t) ((uint32_t) 1<<8))
#define UART0_RX_PORTB_FER ((uint32_t) ((uint32_t) 1<<9))

#define SPI1_CLK_PORTA_MUX ((uint32_t) ((uint32_t) 0<<0))
#define SPI1_MISO_PORTA_MUX ((uint32_t) ((uint32_t) 0<<2))
#define SPI1_MOSI_PORTA_MUX ((uint32_t) ((uint32_t) 0<<4))
#define SPI1_SEL1_PORTA_MUX ((uint32_t) ((uint32_t) 0<<8))

#define SPI1_CLK_PORTA_FER ((uint32_t) ((uint32_t) 1<<0))
#define SPI1_MISO_PORTA_FER ((uint32_t) ((uint32_t) 1<<1))
#define SPI1_MOSI_PORTA_FER ((uint32_t) ((uint32_t) 1<<2))
#define SPI1_SEL1_PORTA_FER ((uint32_t) ((uint32_t) 1<<4))

#define SPI2_CLK_PORTB_MUX ((uint32_t) ((uint32_t) 0<<20))
#define SPI2_MISO_PORTB_MUX ((uint32_t) ((uint32_t) 0<<22))
#define SPI2_MOSI_PORTB_MUX ((uint32_t) ((uint32_t) 0<<24))
#define SPI2_SEL1_PORTB_MUX ((uint32_t) ((uint32_t) 0<<30))

#define SPI2_CLK_PORTB_FER ((uint32_t) ((uint32_t) 1<<10))
#define SPI2_MISO_PORTB_FER ((uint32_t) ((uint32_t) 1<<11))
#define SPI2_MOSI_PORTB_FER ((uint32_t) ((uint32_t) 1<<12))
#define SPI2_SEL1_PORTB_FER ((uint32_t) ((uint32_t) 1<<15))

int32_t adi_initpinmux(void);

/*
* Initialize the Port Control MUX and FER Registers
*/
int32_t adi_initpinmux(void)
{
/* PORTx_MUX registers */
*pREG_PORTB_MUX = UART0_TX_PORTB_MUX | UART0_RX_PORTB_MUX;

/* PORTx_FER registers */
*pREG_PORTB_FER = UART0_TX_PORTB_FER | UART0_RX_PORTB_FER;

/* PORTx_MUX registers */
*pREG_PORTB_MUX = SPI2_CLK_PORTB_MUX | SPI2_MISO_PORTB_MUX
| SPI2_MOSI_PORTB_MUX | SPI2_SEL1_PORTB_MUX;

/* PORTx_FER registers */
*pREG_PORTB_FER = SPI2_CLK_PORTB_FER | SPI2_MISO_PORTB_FER
| SPI2_MOSI_PORTB_FER | SPI2_SEL1_PORTB_FER;

/* PORTx_MUX registers */
*pREG_PORTA_MUX = SPI1_CLK_PORTA_MUX | SPI1_MISO_PORTA_MUX
| SPI1_MOSI_PORTA_MUX | SPI1_SEL1_PORTA_MUX;

/* PORTx_FER registers */
*pREG_PORTA_FER = SPI1_CLK_PORTA_FER | SPI1_MISO_PORTA_FER
| SPI1_MOSI_PORTA_FER | SPI1_SEL1_PORTA_FER;

return 0;
}

Transmitter:
*pREG_SPI1_SLVSEL &= ~ENUM_SPI_SLVSEL_SSEL1_HI ; // select device

while(!(*pREG_SPI1_STAT & BITM_SPI_STAT_RFE)) *pREG_SPI1_RFIFO;

*pREG_SPI1_TWC = 1; // single byte instruction, no addr/data
*pREG_SPI1_TFIFO = 0xAA; // command ID
while(!(*pREG_SPI1_STAT & BITM_SPI_STAT_TF)); // wait till completion
*pREG_SPI1_STAT = BITM_SPI_STAT_TF; // clear latch
while(*pREG_SPI1_STAT & BITM_SPI_STAT_RFE);

*pREG_SPI1_SLVSEL |= ENUM_SPI_SLVSEL_SSEL1_HI ; // select device

But SPI1 does not work, can help or
opinion?

Thanks!