Hi!
I'm using custom board with bf704 and ICE-1000 emulator.
All jtag tests are successful. But when i'm working in CCES 2.3 getting the following error messages:
" Attempting to connect to an unknown device, however session is for a ADSP-BF704."
"Error in launch sequence [TpsdkServer] Failed to halt processor 0"
I checked all the power supply voltage, checked a quartz resonator signal.
i'm using 14-pin connector with the following signals:
What can lead to this error?
Thanks.