bf706 image acquisition question

Hi ADI's

using BF706 and having a strange problem.
The BF706 is receiving images through the cmos chip.
The size is 640 * 480.
When receive the first RAW image, a black line will appear at the bottom. RAW data received from the frame buffer.
I wonder why this is happening.
Because of this, if you resize an image of 640 * 480, you will see a line next to the image.
The attached fp.png file is a 640 * 480 RAW file captured on the monitor screen
Attaches RAW image data.

<Process flow>
1. Run the imc_configure function at boot time to set the EPPI (run once at boot time)
     sys-> fplib-> fpimage is a frame buffer.
     imc-> cb.dwframeWidth = 640
     imc-> cb.dwframeHeight = 480
 
2. Execute imc_open () and execute imc_capture () after capturing Execute sys-> fplib-> fpimage Import frame data from frame buffer to 640 * 480 size. Fpimg1.raw with the data attached and fp.png from the viwer program.
 
Please make sure that there is a problem in the code regarding the problem that black bold line appears at the bottom of the image.
 
I suspect that the frame buffer memory is bad.
Frame buffer size is larger than 640 * 480 size

imc_configure

//----------------------------------------------------------------------------
//          Blackfin ADSP-BF706
//----------------------------------------------------------------------------
// File Name           : _imc.c
// Project             : FAS06_v2.0
// Generated           : by UNION COMMUNITY Co.,Ltd. 2016.05.10
//----------------------------------------------------------------------------

#include "global.h"

#define _USE_IMC_CACHE_ATTRIBUTE
#define IMC_PRINTF(s)	CON_PRINTF(s)

static struct imcinfo __imcinfo__;

REG_EPPI_DMA* EPPI_DMA = (REG_EPPI_DMA*)DMACH0_REG_BASE;
REG_EPPI* EPPI = (REG_EPPI*)EPPI_REG_BASE;

static void imc_enable(void)
{
	EPPI_DMA->cfg |= (ENUM_DMA_CFG_SYNC|ENUM_DMA_CFG_EN);
	EPPI->ctl |= ENUM_EPPI_CTL_EN;
}

static void imc_disable(void)
{
	EPPI_DMA->cfg &= ~ENUM_EPPI_CTL_EN;
	EPPI->ctl &= ~ENUM_EPPI_CTL_EN;
}

struct imcinfo *getimcinfo(void)
{
	return &__imcinfo__;
}

static void imc_irq (uint32_t iid, void* handlerArg)
{
	struct imcinfo *imc = getimcinfo();

	if(EPPI_DMA->stat | BITM_DMA_STAT_IRQDONE)
	{
		imc_close();
		EPPI_DMA->stat = BITM_DMA_STAT_IRQDONE;
		imc->cb.eState = IMC_STATE__COMPLATE;
	}
}

u32 imc_capture(void)
{
	struct imcinfo *imc = getimcinfo();

	imc_enable();
	EPPI_DMA->stat = BITM_DMA_STAT_IRQDONE;
	adi_int_EnableInt(imc->irq, true);

	watchdog_signal();

	imc->cb.eState = IMC_STATE__READY;

	while(1)
	{
		if(imc->cb.eState == IMC_STATE__COMPLATE)
		{
			imc->cb.eState = IMC_STATE__NULL;

			break;
		}
	}
	adi_int_EnableInt(imc->irq, false);

	return IMC_SUCCESS;
}

void imc_close(void)
{
	struct imcinfo *imc = getimcinfo();

	watchdog_signal();

	imc_disable();
}

u32 imc_configure(void)
{
	struct imcinfo *imc = getimcinfo();
	struct sysinfo *sys = getsysinfo();

	if(imc->cb.eState == IMC_STATE__NULL)
		return IMC_ERR_INVALID_STATE;

	// EPPI DMA Channel1 Setting
	EPPI_DMA->addr_start = (u32) sys->fplib->fpimage;

	EPPI_DMA->cfg = 0x00000000;
	EPPI_DMA->cfg = ENUM_DMA_CFG_ADDR2D | ENUM_DMA_CFG_YCNT_INT | ENUM_DMA_CFG_STOP | //ENUM_DMA_CFG_AUTO | ENUM_DMA_CFG_STOP |
			ENUM_DMA_CFG_PSIZE04 | ENUM_DMA_CFG_MSIZE04 | ENUM_DMA_CFG_WRITE | ENUM_DMA_CFG_SYNC | ENUM_DMA_CFG_DIS;

	EPPI_DMA->xcnt = imc->cb.dwframeWidth/4;
	EPPI_DMA->xmod = 4;

	EPPI_DMA->ycnt = imc->cb.dwframeHeight;
	EPPI_DMA->ymod = 4;

	// EPPI Setting
	EPPI->imsk = 0xFF;

	EPPI->ctl = 0x00000000;
	EPPI->ctl = ENUM_EPPI_CTL_DMA1CHAN | ENUM_EPPI_CTL_PACK_EN | ENUM_EPPI_CTL_DLEN08 | ENUM_EPPI_CTL_FS1HI_FS2HI |
			ENUM_EPPI_CTL_POLC00 | ENUM_EPPI_CTL_FLDSEL_HI | ENUM_EPPI_CTL_SYNC2 | ENUM_EPPI_CTL_NON656 |
			ENUM_EPPI_CTL_RXMODE | ENUM_EPPI_CTL_DIS;

	EPPI->hcnt = imc->cb.dwframeWidth;
	EPPI->line = imc->cb.dwframeWidth;

	EPPI->vcnt = imc->cb.dwframeHeight;
	EPPI->frame = imc->cb.dwframeHeight;

	imc->cb.eState = IMC_STATE__READY;

	return IMC_SUCCESS;
}

u32 imc_open(void)
{
	u32		ret;
	struct imcinfo *imc = getimcinfo();

	imc->cb.eState = IMC_STATE__INIT;

	//ret = imc_configure();
	return ret;
}

void imc_init(int mode)
{
	struct imcinfo*	imc = getimcinfo();
	struct sysinfo*	sys = getsysinfo();
	
	// zero-initialize info block
	kbzero(imc,sizeof(struct imcinfo));

	if(sys->config.fpapi.sensor == FS_FCS06)
	{
		// FCS06 센서일 경우
		imc->config.eSrcImgType		= IMC_SRC_IMG__GRAY;

		// default 640*480 시작 좌표는 (80,8) 이지만 CMOS를 셋팅했으므로 (0,0)이다.
		imc->config.dwLeftWnd		= 0;
		imc->config.dwTopWnd		= 0;
		imc->config.dwRightWnd		= IMC_SRC_WIDTH_SIZE-1;	//0+640-1;
		imc->config.dwBottomWnd		= IMC_SRC_HEIGHT_SIZE-1;	//0+480-1;

		imc->cb.dwframeWidth		= IMC_MAX_ACTIVE_WIDTH_SIZE;
		imc->cb.dwframeHeight		= IMC_MAX_ACTIVE_HEIGHT_SIZE;
		imc->cb.dwframeSize			= (IMC_MAX_ACTIVE_WIDTH_SIZE * IMC_MAX_ACTIVE_HEIGHT_SIZE);

		imc->cb.eState				= IMC_STATE__INIT;
	}

	imc_configure();

	imc->irq = INTR_EPPI0_CH0_DMA;

	adi_int_InstallHandler(imc->irq, imc_irq, NULL, false);
}

imc.h

//----------------------------------------------------------------------------
//          Pixelplus PM1002K
//----------------------------------------------------------------------------
// File Name           : imc.h
// Project             : FAS02NL2
// Generated           : by UNION COMMUNITY Co.,Ltd. 2008.10.10
//----------------------------------------------------------------------------
#ifndef __IMC_H__
#define __IMC_H__

/*! Memory required for the ov7692 sensor driver itself excluding the memory required by its dependent drivers */
#define IMC_SELF_MEMORY_SIZE        70

/*!
 * Memory required for the operation of OV7692 driver in bytes.
 */
//#define IMC_MEMORY_SIZE             (IMC_SELF_MEMORY_SIZE + IMC_EPPI_MEMORY_SIZE + ADI_TWI_MEMORY_SIZE)

#define IMC_MAX_ACTIVE_WIDTH_SIZE		FULL_WIDTH
#define IMC_MAX_ACTIVE_HEIGHT_SIZE		FULL_HEIGHT

#define IMC_SRC_WIDTH_SIZE		FULL_WIDTH
#define IMC_SRC_HEIGHT_SIZE		FULL_HEIGHT

/*! Number of bytes required to store the pixel. */
#define IMC_BYTES_PER_PIXEL         2
#define IMC_Y_BYTES_PER_PIXEL       1

/*! Number of registers needed to configure the size */
#define IMC_IMAGE_CFG_ARRAY_SIZE    14

#define IMC_SUCCESS 						0
#define IMC_ERR_INVALID_SIZE				1
#define IMC_ERR_INVALID_STATE				2
#define IMC_ERR_BUS_ERROR					3
#define IMC_ERR_MEM_OVERFLOW				4
#define IMC_ERR_FIFO_FULL					5
#define IMC_FAIL_ERROR 						6

/*
 * DMA Register Set
 */

#define DMACH0_REG_BASE				0x2008A000
#define DMACH1_REG_BASE				0x2008B000

typedef struct _REG_EPPI_DMA_ {
	VULONG	dscptr_nxt;
	VULONG	addr_start;
	VULONG	cfg;
	VULONG	xcnt;
	VULONG	xmod;
	VULONG	ycnt;
	VULONG	ymod;
	VULONG	Reserved1;
	VULONG	Reserved2;
	VULONG	dscptr_cur;
	VULONG	dscptr_prv;
	VULONG	addr_cur;
	VULONG	stat;
	VULONG	xcnt_cur;
	VULONG	ycnt_cur;
}REG_EPPI_DMA;

/*
 * EPPI Register Set
 */

#define EPPI_REG_BASE				0x20063000

typedef struct _REG_EPPI_ {
	VULONG	stat;
	VULONG	hcnt;
	VULONG	hdly;
	VULONG	vcnt;
	VULONG	vdly;
	VULONG	frame;
	VULONG	line;
	VULONG	clkdiv;
	VULONG	ctl;
	VULONG	fs1_wlhb;
	VULONG	fs1_paspl;
	VULONG	fs2_wlvb;
	VULONG	fs2_paspf;
	VULONG	imsk;
	VULONG	oddclip;
	VULONG	evenclip;
	VULONG	fs1_dly;
	VULONG	fs2_dly;
	VULONG	ctl2;
}REG_EPPI;


typedef enum
{
	IMC_STATE__NULL = 0,
	IMC_STATE__INIT,
	IMC_STATE__READY,
	IMC_STATE__CAPTURING,
	IMC_STATE__COMPLATE,
	IMC_STATE__ERROR
} IMC_STATE_TYPE;

// Image mode
typedef enum
{
	IMC_SRC_IMG__GRAY = 0,
	IMC_SRC_IMG__BAYER = 1,
	IMC_SRC_IMG__YCbCr
} E_IMC_SRC_IMG_TYPE;

// Type of column/row line sub-sample scale from orignal image(window size).
typedef enum
{
	IMC_SMP_SCL__DIV_1	 = 0,
	IMC_SMP_SCL__DIV_2	 = 1,
	IMC_SMP_SCL__DIV_4	 = 2,
	IMC_SMP_SCL__DIV_8	 = 3,
	IMC_SMP_SCL__DIV_16  = 4,
	IMC_SMP_SCL__DIV_32  = 5,
	IMC_SMP_SCL__DIV_64  = 6,
	IMC_SMP_SCL__DIV_128 = 7
} E_IMC_SMP_SCL_TYPE;

// Source type of input image.
typedef enum
{
	IMC_SMP_SRC_EXT = 0,
	IMC_SMP_SRC_FRMMEM = 2,
	IMC_SMP_SRC_IPOL = 5
} E_IMC_SMP_SRC_PATH;

// Bayer pattern 
typedef enum
{
	IMC_BAYER_PAT__RGRG = 0,
	IMC_BAYER_PAT__GBGB = 1,
	IMC_BAYER_PAT__GRGR = 2,
	IMC_BAYER_PAT__BGBG = 3,
	IMC_BAYER_PAT__NONE = 4 
} E_IMC_BAYER_PAT_TYPE;

// Source of Writing data
typedef enum
{
	IMC_WRITE_SRC__EXT = 0, 
	IMC_WRITE_SRC__SUBSAM, 
	IMC_WRITE_SRC__IPOL
} E_IMC_WRITE_SRC_PATH;

// Source of output data to use HV, BDU...
typedef enum
{
	IMC_OUTPUT_SRC__EXT = 0,
	IMC_OUTPUT_SRC__SUBSAM,
	IMC_OUTPUT_SRC__FRMMEM,
	IMC_OUTPUT_SRC__IPOL
} E_IMC_OUTPUT_SRC_PATH;

// Source of bayer interpolation 
typedef enum
{
	IMC_IPOL_SRC__EXT = 0,
	IMC_IPOL_SRC__SUBSAM,
	IMC_IPOL_SRC__FRMMEM,
	IMC_IPOL_SRC__NONE
} E_IMC_IPOL_SRC_PATH;

struct imcinfo {
	int					type;
	bool				open;
	u32					irq;

	struct {
		u32				eSrcImgType;
		u32				dwLeftWnd;		// x-coordinate of the upper-left corner on the rectangle
		u32 			dwTopWnd;		// y-coordinate of the upper-left corner on the rectangle
		u32 			dwRightWnd;		// x-coordinate of the lower-right corner on the rectangle
		u32 			dwBottomWnd;	// y-coordinate of the lower-right corner on the rectangle
	} config;

	struct {
		u32				dwframeWidth;
		u32				dwframeHeight;
		u32				dwframeSize;
		u32				dwWndWidth;
		u32		 		dwWndHeight;
		IMC_STATE_TYPE	eState;
	} cb;
};

struct imcinfo *getimcinfo(void);
u32 imc_capture(void);
void imc_close(void);
u32 imc_open(void);
void imc_init(int mode);

#endif //__IMC_H__

Thank you



tagged
[edited by: JValeriani at 3:09 PM (GMT 0) on 14 Oct 2019]
Parents Reply Children
No Data