ADSP-BF706
Production
This device is a member of the ADSP-BF70x Blackfin Digital Signal Processor (DSP) product family. The new Blackfin+ processor core combines dual-MAC 16...
Datasheet
ADSP-BF706 on Analog.com
I have an audio in-out program in C for the ADSP-BF706 EZ-KIT mini, about 80 lines in length. It's simple and very easy to understand. It's also completely self-contained - it doesn't use any of the header files that the "TalkThrough_BF706Mini.c" program uses (supplied with the kit). It includes a basic TWI driver, SPORT0 set up and configuration routine for the on board codec (ADAU1761). With some simple modifications it can be used for filtering, both FIR and IIR. The file is attached. All welcome to use free.
PatrickG
Why is double buffering necessary? I have clearly showed a method in my
samples that uses DMA in circular mode and the DMA runs itself without
double-buffering assistance. Of course the DMA can also run in linked list
mode, but it's not like you are submitting data where you need write behind
via page flipping mode like you do in graphics...There is a way to setup
the DMA to run circular with very large chunks of audio...Even 1 second
long!
On Sat, Jul 14, 2018, 9:29 AM UweS <analog@analog-vm.hosted.jivesoftware.com>
Why is double buffering necessary? I have clearly showed a method in my
samples that uses DMA in circular mode and the DMA runs itself without
double-buffering assistance. Of course the DMA can also run in linked list
mode, but it's not like you are submitting data where you need write behind
via page flipping mode like you do in graphics...There is a way to setup
the DMA to run circular with very large chunks of audio...Even 1 second
long!
On Sat, Jul 14, 2018, 9:29 AM UweS <analog@analog-vm.hosted.jivesoftware.com>