I have an audio in-out program in C for the ADSP-BF706 EZ-KIT mini, about 80 lines in length. It's simple and very easy to understand. It's also completely self-contained - it doesn't use any of the header files that the "TalkThrough_BF706Mini.c" program uses (supplied with the kit). It includes a basic TWI driver, SPORT0 set up and configuration routine for the on board codec (ADAU1761). With some simple modifications it can be used for filtering, both FIR and IIR. The file is attached. All welcome to use free.
PatrickG
Here is BF706_Audio_v3.zip
Hello Patrick !
That is I need for my first BF706 project on my own dsp board.
Thank you !
Roman
Hello Patrick,
your program for the BF706 EZ-Kit Lite is very useful, very clear and it works fine!I have written a DMA and interrupt driven version to avoid polling. This could be a first step to block…
Hallo Patrick,
my BF706 audio filter program has a bug. The lines
if (*pREG_DMA1_STAT & ENUM_DMA_STAT_IRQDONE) *pREG_DMA1_STAT = ENUM_DMA_STAT_IRQDONE;
are missing in the SPORT0_RX_interrupt_handler.
Maybe this is useful for the development of your own DMA interrupt software.
The attached version BF706_Audio_Filter_v2 should be correct.
Best regards
Uwe