Article ADSP BF706 Ezkit Mini SPI1 cannot be done in master mode.

BF706 Ezkit Mini SPI port on P5 has a line buffer which is connected, This line buffer does not work properly if we use the DSP as master.

 

This is due to The board is setup for a SPI device plugged into the P5 connector to drive the signal and not the BF706.  The buffer would need to be removed and the two signals shorted together in order to driving the signal from the BF706.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.