Article How the System Cross Bar (SCB) in BF70x different than in BF60x ?

The SCB fabric in BF70x has the following major differences as compared to that in BF60x:

- The SCB arbitration in BF60x is programmed in terms of number of read/write channel slots while in BF70x, the arbitration is programmed in terms of the read/write Quality of Service (OQS) value. Each master is associated with its own read/write QOS value. This value is used by the SCBs at various levels to arbitrate among various masters. For more details, please refer BF70x HRM.

- The SCB fabric in BF70x has "Interface Block Sync Mode" registers to program the clock domain crossing (async/1:1/1:n/n:1) across various clock domains (e.g. SYSCLK:DCLK, SCLK1:SYSCLK etc). This helps in improving the throughput across the fabric. This option is not available in BF60x.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.