Processor: ADSP-BF70x All the DMA error interrupts are combined into a single shared interrupt. Combined error signals require reading the DMA_STAT register of each DMA channel associated with a combined…
ADSP-BF60x/BF70x features CRC32 protection is implemented in hardware. The boot kernel provides mechanisms to allow each block to be verified using a 32-bit CRC.
When building a LDR file for CRC32 protection…
Question:
I have a BF70x application which cannot boot in secure mode. The same application boots without issue using non-secure mode
-----------------------------
Answer:
ADSP-BF70x processors…
For the discussion of ADSP-BF70x processors, peripherals, programming, applications and hardware design.
Please read the Analog Devices EngineerZone Code of Conduct before posting.
1. Instruction Cache Way Locking:
The instruction cache way locking feature is no longer supported in new Blackfin+ core.
2. Direct access to cache and Instruction memory space:
Blackin+ processor…
Q:
Can I pass the output generated from PKA directly to the PKTE module for encryption/decryption?
--------------
A:
No, this cannot be done directly as PKTE supports Little Endian format whereas…
In single-pulse PWMOUT mode, the timer generates a single pulse on the TIMER_TMR[n] pin. This mode is frequently used to implement a precise delay, often with generating an output trigger. In continuous…
1. CPLB default MMRS
New MMRs are added to take specific default action when data or instruction CPLBs are missed. A default cache mode, memory properties, access restrictions can be programmed in…
The attached code implements the digital watch functionality using the RTC. For the ease of use,the code accepts the date and time in Sec:Min:Hr DD/MM/YR format and get the date and time from RTC in same…