Join us for an exciting webinar where we will unveil and demonstrate our new bulk ordering and bulk quoting tools! Discover how you can streamline your...
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
      1. First, the quote of the week: " The best measure of a man's honesty isn't his income tax return. It's the zero adjust on his bathroom scale " - Unknown...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: White Coats and Multi-Coloured Pens Ready to put...
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
    I discuss various aspects of the SFF (safe failure fraction) —whether it applies to an integrated circuit —and whether an integrated circuit can have more...

     

    Powering the Future: Multiphase Buck-Boost Innovation for Telecom: Part 3 of 3

    How can we meet the growing power requirements of the future? 5G network deployments necessitate high-efficiency power conversion solutions capable of...
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
ADSP-BF60x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF60x
  • Processors and DSP
  • Blackfin Processors
  • ADSP-BF60x
  • Cancel
ADSP-BF60x
Documents Booting from SDRAM for ADSP-BF60x Blackfin using rom_Boot api
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP-BF609: FAQ
  • -ADSP-BF60x: FAQ
    • ADSP-BF60X BLACKFIN PROCESSOR SUPPORT COMMUNITY
    • Booting from SDRAM for ADSP-BF60x Blackfin using rom_Boot api
    • Example code for CRC ADSP-BF60x
    • How to Configure BF60x Watchdog as SEC Fault or interrupt on watchdog count expiry to do manual reset
    • What software development tools are available for the ADSP-BF60x processors?
    • Where can I find information about the Blackfin ADSP-BF60x processors?
    • Where can I find power consumption data for BF60x processors?
    • Where can I find the latest preliminary AC specifications for BF60x processors?
    • ​​​​​ Second-Stage Loaders for ADSP-BF60x Blackfin using Memory boot mode
  • EPPI example for BF609
  • How to identify the state of the processor during crash?
  • Troubleshooting SPI Master Boot Halt: Managing Block Size for Stability in ADSP-BF609

Booting from SDRAM for ADSP-BF60x Blackfin using rom_Boot api


Please follow the below steps to boot from SDRAM:

1. Create loader file for simple led dual core application with below options:
Boot mode   : Memory
boot format : Include
width           : 8 bit
Boot code   : 0x1

2. In ROM application, Store the loader file at SDRAM and call ROM api as below.
rom_Boot(0x02000000,0,0,0,ENUM_ROM_BCMD_DEVICE_MEMORY,0);

0x02000000                  - address of DDR2
ENUM_ROM_BCMD_DEVICE_MEMORY - Memory booting

3. Debug the ROM application, it runs the led application from SDRAM. Please refer the attached example.

SSL_SDRAM_boot.zip

  • Share
  • History
  • More