Post Go back to editing

Wrong information in Hardware Reference

Hi,

I've found an wrong information in the Hardware Reference Manual of the BF609.

On Page 21-32 section "Mailbox Direction 1 Register" the text says "...set the bit (=1) for transmit mode from the mailbox..."

Actually the bit has to set to "0" that the mailbox operates in transmit mode.

Thomas

Parents
  • Thanks! I already thought so. I was just wondering about the text in the manual (page 21-82:

         "Mailbox ID 1 Register

         The CAN_MBnn_ID1 register and CAN_MBnn_ID0 register manage acceptance mask operations. For      information about acceptance mask operation, see the Receive Operation section."

Reply
  • Thanks! I already thought so. I was just wondering about the text in the manual (page 21-82:

         "Mailbox ID 1 Register

         The CAN_MBnn_ID1 register and CAN_MBnn_ID0 register manage acceptance mask operations. For      information about acceptance mask operation, see the Receive Operation section."

Children
No Data