Post Go back to editing

Wrong information in Hardware Reference

Hi,

I've found an wrong information in the Hardware Reference Manual of the BF609.

On Page 21-32 section "Mailbox Direction 1 Register" the text says "...set the bit (=1) for transmit mode from the mailbox..."

Actually the bit has to set to "0" that the mailbox operates in transmit mode.

Thomas

Parents
  • The 11-bit BaseID should be set in CAN_MBxx_ID1[12:2] field.

    The 18-bit Extended ID should be specied in CAN_MBxx_ID1[1:0] and CAN_MBxx_ID0[15:0] fields. The upper 2-bits in ID1 register and remaining 16-bits in ID0 register.

    This is same settings as in previous Blackfin processor's CAN module.

Reply
  • The 11-bit BaseID should be set in CAN_MBxx_ID1[12:2] field.

    The 18-bit Extended ID should be specied in CAN_MBxx_ID1[1:0] and CAN_MBxx_ID0[15:0] fields. The upper 2-bits in ID1 register and remaining 16-bits in ID0 register.

    This is same settings as in previous Blackfin processor's CAN module.

Children
No Data