bf609 , how to boot dual-core application ?

Hello ,

My question : how to boot dual-core application from different location in Flash memory ?

Enviroment : BF609-EZKIT , CCES 1.0.3.0 , emulator 100B or HPUSB-ICE

1. I wrote simple dual-core application , i.e. LED Blink  :

           Core0 - LED 1 and LED 2 on the BF609-EZKIT board

           Core1 - LED 3 and LED 4 on the BF609-EZKIT board

2. My CCES setup for dual core-application (in Post-build steps field)

elfloader.exe -proc ADSP-BF609 -si-revision 0.1 -b MEMORY -f binary -width 16 -bcode 0x01 C:\CCES\App_Core0\Debug\App_Core0.dxe -NoFinalTag C:\CCES\App_Core1\Debug\App_Core1.dxe  -o c:\tftp-root\prog0.ldr

It means that I link 2 *.dxe files into one *.ldr file  (prog0.ldr) . In LdrViewer it is visible as multi-dxe structure (2 dxe blocks) without Final Flag after first block. So it looks good.

3. If I run this application via Emulator : it works OK !!! (both cores OK )

4. If I programmed prog0.ldr file into default location in Flash memory ( 0xb0000000) and press RESET :  it works OK !!!  (both cores OK)

5. If I programmed prog0.ldr file into any different location ( i.e. 0xb0100000 ) and I tried to use rom_Boot () function it DOESN'T WORK !!!

   ( none core doesn't work !!!!)

Example of use rom_Boot()  function below :

#define _BOOTROM_MEMBOOT  0xC800000C

int (*BOOTROM_MEM)(void *, int, int, void *, int , void *) =  (void *) _BOOTROM_MEMBOOT;      // => 0xC800000C

BOOTROM_MEM(0xb0100000 , 0x00, 0 , NULL, 0x01,NULL);    (call rom_BOOT () function !!!)

I checked a lot of argument combinations in the BOOTROM_MEM () function call , but without any success .

6. If I use the same method for booting single-core application it works OK !!!

    (but only when the application doesn't  include InitCode !!! ) .

    The application with InitCode included looks like multi-dxe application ( has got 2 dxe blocks)

    May be it is similar problem ?

So I am surprise why the same file ( prog0.ldr ) works properly from default location but doesn't work from any other ?

I'd like to write a Second Stage Loader Application and I very need this possibility .

Where is the problem ?  Could anybody help me , please ?

Thank you in advance

Jaroslaw

Parents
  • Hello ,

    I solved this problem. The solution is simple but unfortunately there is no way to find it in any docs !!!

    I spent a lot of time to do it.

    Here it is:  Your calling application MUST be dual-core application too !!!

    So (as in my case) , if you use U-boot bootloader as calling application it will not work !!!

    By default u-boot is built as a single-core application and you MUST change u-boot to dual-core application !!!

    I performed following steps:

    1. Rebuilt u-boot code (in Linux enviroment) with defined :

    #define CONFIG_CORE1_RUN    1 << uncomment this line !!!

    2. Merge obtained  u-boot code  (u-boot)  with any Core 1 application (Uboot_Core1.dxe) as follow:

    bfin-elf-ldr -T bf609 -c u-boot2.ldr u-boot Uboot_Core1.dxe --bmode PARA --use-vmas --initcode arch/blackfin/cpu/initcode.o  -J --punchit $((0x8000)):$((0x8000)):env-ldr.o

    3. In result we obtained dual-core u-boot2.ldr application

    4. This application can boot another dual-core application !!!!

    May be it will be usefull for somebody

    Regards

    Jaroslaw

Reply
  • Hello ,

    I solved this problem. The solution is simple but unfortunately there is no way to find it in any docs !!!

    I spent a lot of time to do it.

    Here it is:  Your calling application MUST be dual-core application too !!!

    So (as in my case) , if you use U-boot bootloader as calling application it will not work !!!

    By default u-boot is built as a single-core application and you MUST change u-boot to dual-core application !!!

    I performed following steps:

    1. Rebuilt u-boot code (in Linux enviroment) with defined :

    #define CONFIG_CORE1_RUN    1 << uncomment this line !!!

    2. Merge obtained  u-boot code  (u-boot)  with any Core 1 application (Uboot_Core1.dxe) as follow:

    bfin-elf-ldr -T bf609 -c u-boot2.ldr u-boot Uboot_Core1.dxe --bmode PARA --use-vmas --initcode arch/blackfin/cpu/initcode.o  -J --punchit $((0x8000)):$((0x8000)):env-ldr.o

    3. In result we obtained dual-core u-boot2.ldr application

    4. This application can boot another dual-core application !!!!

    May be it will be usefull for somebody

    Regards

    Jaroslaw

Children
No Data