Hi guys,
I want to use Linkport0, Linkport1 and SMC at the same time, it seems to be have pin conflict problem.
The address signals are pinmuxed with Linkport0/1's data signal.
The question is, can I use the other GPIOs to simulate the address signal of the SMC to work around this problem?
The peripheal on the SMC is a FPGA and therefore the address decode can be flexible...
(On the other word, only the SMC control signal like AMS0, "read/write enable"... are still available, and all the address signals will not be used).
Any one can give me a quick answer for that?! Thanks a lot!
Ken