Hi,
The platform is BF609.
The scenario is PPI0--> PVP--> Core0.
We use 3 PVP streams: Threshold, Sobel X, Sobel Y.
The bank configuration as bellow:
//================================================================================code begine=======================================
#pragma section ("sdram_bank7")
static int16_t GxOutBuf[PEC_OUT_BUF_SIZE];
#pragma section ("sdram_bank7")
static int16_t GxOutBuf1[PEC_OUT_BUF_SIZE];
#pragma section ("sdram_bank7")
static int16_t GxOutBuf2[PEC_OUT_BUF_SIZE];
#pragma section ("sdram_bank6")
static int16_t GyOutBuf[PEC_OUT_BUF_SIZE];
#pragma section ("sdram_bank6")
static int16_t GyOutBuf1[PEC_OUT_BUF_SIZE];
#pragma section ("sdram_bank6")
static int16_t GyOutBuf2[PEC_OUT_BUF_SIZE];
#pragma section ("sdram_bank4")
static uint8_t THCOutBuf[PEC_OUT_BUF_SIZE];
#pragma section ("sdram_bank4")
static uint8_t THCOutBuf1[PEC_OUT_BUF_SIZE];
#pragma section ("sdram_bank4")
static uint8_t THCOutBuf2[PEC_OUT_BUF_SIZE];
//======================================================================code ends================================================================
In this allocation, we avoid the conflict from Different PVP streams trying to write to a same bank.
But we cannot guarantee conflict between Core0 and PVP.
Problem:
When we check the output three img, which are Bina IMG, Sobel X IMG, Sobel Y IMG, for nearly every 30 frames, we observe a strange shift in either one img.
I notice in other forum and here that some guy met the same problem. In his words, this bad thing happen as long as >3 DMA are used. (No matter SCB slots reallocation)
I wonder what is the real reason ? Have you ever handle the same case?