Wrong information in Hardware Reference

Hi,

I've found an wrong information in the Hardware Reference Manual of the BF609.

On Page 21-32 section "Mailbox Direction 1 Register" the text says "...set the bit (=1) for transmit mode from the mailbox..."

Actually the bit has to set to "0" that the mailbox operates in transmit mode.

Thomas

Parents
    •  Analog Employees 
    on Feb 6, 2013 9:52 PM

    That text is also incorrect, and we will make sure it also gets addressed in the next revision of the manual.  The supporting text for the ID0/1 register pair should be describing that these registers define the function of the mailbox, whether it is a specific message ID or a group of message IDs.

Reply
    •  Analog Employees 
    on Feb 6, 2013 9:52 PM

    That text is also incorrect, and we will make sure it also gets addressed in the next revision of the manual.  The supporting text for the ID0/1 register pair should be describing that these registers define the function of the mailbox, whether it is a specific message ID or a group of message IDs.

Children
No Data