Hello everyone
I am using ADSP-CM408 can not communicate with the JLINK, can not download the program, the picture is as follows:
1, VREG_BASE, VDD_VREG Connect to the ground, the use of external power (VDD_INT 1.2V).
2, SYS_RESOUT, SYS_FAULT connected the 10K resistor to 3.3V.
3, SYS_BMODE0, SYS_BMODE1 connected the 10K resistor to the ground, without the use of boot mode.
4, SYS_NMI connection 10K resistance to 3.3V.
5, VDD_INT=1.2V
6, VDD_EXT=3.3V
7, VDD_ANA0,VDD_ANA1=3.3V
8, JLINK is normal.