This webinar will introduce remote-controlled edge nodes and how they promise to simplify the automotive network architecture and expedite the integration...
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
      1. Quote of the week: "Knowledge is knowing a tomato is a fruit. Wisdom is not putting it in a fruit salad" - unknown Sources: commons.wikimedia...

    View All

    What's Brewing

      Quiz! Why a Hybrid Approach Works Blog and Test Your Knowledge

      Quiz! Understand ISO 26262 Compliance Test your knowledge with our quick quiz , based on the blog " Safety in Layers: Why a Hybrid Approach Works ...
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
    The Limitation of Heat Dissipation IO-Link is used across many branches of factory automation, and in these applications, areas of the factory floor...

     

    GMSL Debugging: Getting a Lock

    Imagine a scenario where you have a brand-new board design or are excited to try out some evaluation kits only to find out that the two devices can’t talk...
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
ADSP-CM40x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-CM40x
  • Processors and DSP
  • ADSP-CM4xxx Processors
  • ADSP-CM40x
  • Cancel
ADSP-CM40x
Documents SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose?
  • Forums
  • Docs/FAQs
  • Members
  • Tags
  • More
  • Cancel
  • Documents
  • +AD CM408F: FAQ
  • +ADSP-CM40x: FAQ
  • +Cache with Async memory connected SRAM: FAQ
  • +Clock to the USB controller: FAQ
  • +MEMX and MEMY physical memories: FAQ
  • +SPI Memory Mapped Mode: FAQ
  • -SPI/Cache: FAQ
    • SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose?
  • +What is XiP: FAQ

SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose?

Wrap mode

Wrap mode is a specific feature supported by most flash devices in market. It enables the host processor to ask for the critical word first in a cache line. If enabled, the core is delivered with the critical word it asked for, as soon as possible (for instance, branching address). When using this mode, the Cache Controller, SPI Controller and the Flash device, all three blocks must be pre-programmed to support the same

 

Line-Wrap mode vs. Line-base-first mode

In Line-base-first mode, the line is always fetched starting at offset 0 (line base) while in line-wrap mode, the critical word is returned first; the rest of the line is fetched with wrap-around addressing. In Line-wrap mode, merging is not possible (not linear). Usually, line-base-first will be faster due to merging.

 

How to decide

Decision is application dependent. User has to experiment with his software, before deciding up on the mode. Some application require that critical instruction be executed very fast, so in such cases Wrap mode maybe used. For typical cases where one wants better linear throughput, Line base first mode maybe a better choice.

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose?
    Sara Collins
    Q SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose? A Wrap mode Wrap mode is a specific feature supported by most flash devices in market. It enables the host processor...
  • SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose?
    MSDAPI
    Question SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose? Answer Wrap mode Wrap mode is a specific feature supported by most flash devices in market. It enables the host processor...
  • RE: ADIN1300 transformerless/capacitive coupling
    EricTP
    Hi Mark, thank you for the feedback. It seems that the key differentiator is current-mode vs. voltage-mode line drivers. Would it be the case that any voltage-mode line driver will tend not have issues...
 
Related Content
  • SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose?
    Sara Collins
    Q SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose? A Wrap mode Wrap mode is a specific feature supported by most flash devices in market. It enables the host processor...
  • SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose?
    MSDAPI
    Question SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose? Answer Wrap mode Wrap mode is a specific feature supported by most flash devices in market. It enables the host processor...
  • RE: ADIN1300 transformerless/capacitive coupling
    EricTP
    Hi Mark, thank you for the feedback. It seems that the key differentiator is current-mode vs. voltage-mode line drivers. Would it be the case that any voltage-mode line driver will tend not have issues...