Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
ADSP-CM40x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-CM40x
  • Processors & DSP
  • ADSP-CM4xxx Processors
  • ADSP-CM40x
  • Cancel
ADSP-CM40x
Documents Can I use MATLAB/Simulink with the ADSP-CM40x?
  • Forums
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD CM408F: FAQ
  • -ADSP-CM40x: FAQ
    • ADSP-CM40x Enablement Package (Rev 2.1.0) Supports Rev H Silicon ONLY
    • ADSP-CM40X PROCESSORS SUPPORT COMMUNITY
    • Analog inputs of internal ADC
    • Can I access ADCM40x cache directly?
    • Can I use MATLAB/Simulink with the ADSP-CM40x?
    • Can the VRef for the ADC on the ADSP-CM40x be used as a voltage supply for other devices?
    • Does AD CM40x feature a Data Cache?
    • Getting Started with ADSP-CM40x Mixed-Signal Control Processors
    • How do I access my ADSP-CM40x 2.0 part when the debugger cannot connect?
    • How do I benchmark or count system cycles of a segemnt of code on the ADSP-CM40x ?
    • What general features of Blackfin Cache are not available in CM40x Cache?
  • +Cache with Async memory connected SRAM: FAQ
  • +Clock to the USB controller: FAQ
  • +MEMX and MEMY physical memories: FAQ
  • +SPI Memory Mapped Mode: FAQ
  • +SPI/Cache: FAQ
  • +What is XiP: FAQ

Can I use MATLAB/Simulink with the ADSP-CM40x?

Question

Can I use MATLAB and Simulink with the ADSP-CM40x and IAR Tool-chain?

==============================

Answer

While there is no direct interface between the IAR Tool-chain and MATLAB or Simulink, Mathworks offer the “Embedded Coder” product, an add-on which can generate portable C/C++ code from a MATLAB algorithm or Simulink model. The code generated from Embedded Coder can be compiled for the ADSP-CM40x processor using the IAR Tool-chain.

Embedded Coder further supports ARM by generating code that is optimized for ARM Cortex-M processors, such as the ADSP-CM40x. This ARM optimized code offers up to a significant execution performance improvement over ANSI/ISO C and supports MATLAB code, Simulink blocks, and DSP System Toolbox filters.

For more information, visit the Embedded Coder Product Page on the Mathworks website.