Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
ADSP-CM40x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-CM40x
  • Processors & DSP
  • ADSP-CM4xxx Processors
  • ADSP-CM40x
  • Cancel
ADSP-CM40x
Documents ADSP-CM40x Enablement Package (Rev 2.1.0) Supports Rev H Silicon ONLY
  • Forums
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD CM408F: FAQ
  • -ADSP-CM40x: FAQ
    • ADSP-CM40x Enablement Package (Rev 2.1.0) Supports Rev H Silicon ONLY
    • ADSP-CM40X PROCESSORS SUPPORT COMMUNITY
    • Analog inputs of internal ADC
    • Can I access ADCM40x cache directly?
    • Can I use MATLAB/Simulink with the ADSP-CM40x?
    • Can the VRef for the ADC on the ADSP-CM40x be used as a voltage supply for other devices?
    • Does AD CM40x feature a Data Cache?
    • Getting Started with ADSP-CM40x Mixed-Signal Control Processors
    • How do I access my ADSP-CM40x 2.0 part when the debugger cannot connect?
    • How do I benchmark or count system cycles of a segemnt of code on the ADSP-CM40x ?
    • What general features of Blackfin Cache are not available in CM40x Cache?
  • +Cache with Async memory connected SRAM: FAQ
  • +Clock to the USB controller: FAQ
  • +MEMX and MEMY physical memories: FAQ
  • +Processors & Microcontrollers
  • +SPI Memory Mapped Mode: FAQ
  • +SPI/Cache: FAQ
  • +What is XiP: FAQ

ADSP-CM40x Enablement Package (Rev 2.1.0) Supports Rev H Silicon ONLY

The ADSP-CM40x Enablement Package (Rev. 2.1.0) software supports only the board revisions stated in the Release Notes and the ADSP-CM40xF device silicon revision H. It does NOT support silicon revisions prior to H; therefore, it must NOT be used in development efforts on older silicon revisions.

The silicon revision is branded on line #3 of the ADSP-CM40xF product package, directly after the lot identification number (e.g., 1234567.1-H indicates that the device is revision H silicon from lot number 1234567.1).

Tags: cm40x cm403 cm408
  • Share
  • History
  • More