Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
ADSP-CM40x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-CM40x
  • Processors & DSP
  • ADSP-CM4xxx Processors
  • ADSP-CM40x
  • Cancel
ADSP-CM40x
Documents How do I access my ADSP-CM40x 2.0 part when the debugger cannot connect?
  • Forums
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD CM408F: FAQ
  • -ADSP-CM40x: FAQ
    • ADSP-CM40x Enablement Package (Rev 2.1.0) Supports Rev H Silicon ONLY
    • ADSP-CM40X PROCESSORS SUPPORT COMMUNITY
    • Analog inputs of internal ADC
    • Can I access ADCM40x cache directly?
    • Can I use MATLAB/Simulink with the ADSP-CM40x?
    • Can the VRef for the ADC on the ADSP-CM40x be used as a voltage supply for other devices?
    • Does AD CM40x feature a Data Cache?
    • Getting Started with ADSP-CM40x Mixed-Signal Control Processors
    • How do I access my ADSP-CM40x 2.0 part when the debugger cannot connect?
    • How do I benchmark or count system cycles of a segemnt of code on the ADSP-CM40x ?
    • What general features of Blackfin Cache are not available in CM40x Cache?
  • +Cache with Async memory connected SRAM: FAQ
  • +Clock to the USB controller: FAQ
  • +MEMX and MEMY physical memories: FAQ
  • +Processors & Microcontrollers
  • +SPI Memory Mapped Mode: FAQ
  • +SPI/Cache: FAQ
  • +What is XiP: FAQ

How do I access my ADSP-CM40x 2.0 part when the debugger cannot connect?

ADSP-CM40x 2.0 processors have a security header which must be correct for the application to run, and for the debugger to be able to connect. If the security header is programmed incorrectly or becomes corrupt, the debugger will be blocked from connecting to the part. The UART Flash Programmer (wsd.exe in the tools directory of the board support package) can be used to mass-erase the flash content, clearing the corrupt header and allowing a clean version of the application to be programmed.

There is a bug in the boot code which affects this mass-erase operation, however – if the security header is corrupt and the key contained within the security is the default key, then:

- The debugger is locked out, as per security requirements;

- The UART interface will incorrectly listen for download of a new application for flash-programming.

- The UART interface will incorrectly not listen for the mass-erase command.

If the security header is corrupt and the key contained within the security is not the default key, then:

- The debugger is locked out, as per security requirements;

- The UART interface will listen for the mass-erase command or a secure key command

The upshot of this is that a part with a corrupt security header will block out the debugger always, but mass-erase over UART will have no effect if the default key is being used.

In the circumstance when the default key is being used, the part can be recovered by:

- Downloading a new application with a valid security header, over the UART.

- Optionally, using the UART Flash Programmer to send the mass-erase command over the UART, if you need to clear the flash.

In the circumstance when a non-default key is being used, the part can be recovered by:

- Sending the mass-erase request to erase the flash, or send the custom key and reprogram a new application

  • Share
  • History
  • More