Post Go back to editing

ADSP-CM409 Download the executable file LED.out

hello, everyone 

I have a question for help,Based on ASDP-CM409 to do a flow lamp procedures,I can realize the function of flow light through J-link Download and debug,But when I downloaded the program into Flash and restarted the development board, the program didn't work.I don't know how to dealwith it,Let me describe my hardware configuration first. Boot Mode Indicates the internal flash mode(01).The design missed the handling of pin.the pin of the sys_resout is dangling,Please help me confirm whether this situation will affect the situation that the program cannot be executed after downloading.at the same time ,I will post the information in the download process below,Hope to get your help, thank you!

log 

Fri Feb 25, 2022 15:32:31: IAR Embedded Workbench 8.32.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\bin\armproc.dll)
Fri Feb 25, 2022 15:32:31: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\config\debugger\AnalogDevices\CM40z.dmac
Fri Feb 25, 2022 15:32:31: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\config\flashloader\AnalogDevices\FlashCM40z.mac
Fri Feb 25, 2022 15:32:31: JLINK command: ProjectFile = D:\Analog Devices\ADSP-CM40x\CM403F_CM408F_EZ-KIT\examples\ADCC_Linear_WPI\iar\settings\adcc_linear_Debug.jlink, return = 0
Fri Feb 25, 2022 15:32:31: Device "ADSP-CM409BSWZ-AF" selected.
Fri Feb 25, 2022 15:32:31: DLL version: V5.12f, compiled May 17 2016 16:03:35
Fri Feb 25, 2022 15:32:31: Firmware: J-Link V11 compiled Aug 14 2019 16:21:09
Fri Feb 25, 2022 15:32:31: Selecting SWD as current target interface.
Fri Feb 25, 2022 15:32:31: JTAG speed is initially set to: 32 kHz
Fri Feb 25, 2022 15:32:31: Found SWD-DP with ID 0x2BA01477
Fri Feb 25, 2022 15:32:31: Found Cortex-M4 r0p1, Little endian.
Fri Feb 25, 2022 15:32:31: FPUnit: 6 code (BP) slots and 2 literal slots
Fri Feb 25, 2022 15:32:32: CoreSight components:
Fri Feb 25, 2022 15:32:32: ROMTbl 0 @ E00FF000
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [0]: FFF0F000, CID: B105E00D, PID: 000BB00C SCS
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [1]: FFF02000, CID: B105E00D, PID: 003BB002 DWT
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [2]: FFF03000, CID: B105E00D, PID: 002BB003 FPB
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [3]: FFF01000, CID: B105E00D, PID: 003BB001 ITM
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [4]: FFF41000, CID: B105900D, PID: 004BB912 TPIU
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [5]: FFF42000, CID: B105900D, PID: 000BB925 ETM
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [6]: FFF43000, CID: B105900D, PID: 002BB914 SWO
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [7]: FFF44000, CID: B105900D, PID: 001BB908 CSTF
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [8]: FFF45000, CID: B105900D, PID: 001BB961 TMC
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [9]: FFF46000, CID: B105900D, PID: 003BB906 ECT / CTI
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [10]: FFF47000, CID: B105900D, PID: 003BB906 ECT / CTI
Fri Feb 25, 2022 15:32:32: ROMTbl 0 [11]: FFF48000, CID: B105900D, PID: 003BB906 ECT / CTI
Fri Feb 25, 2022 15:32:32: Found SWD-DP with ID 0x2BA01477
Fri Feb 25, 2022 15:32:33: Warning: CM40x (reset): Timeout. Core did not halt after reset. Halting CPU manually.
Fri Feb 25, 2022 15:32:33: Hardware reset with strategy 3 was performed
Fri Feb 25, 2022 15:32:33: Initial reset was performed
Fri Feb 25, 2022 15:32:35: 768 bytes downloaded (7.98 Kbytes/sec)
Fri Feb 25, 2022 15:32:35: Loaded debugee: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\config\flashloader\AnalogDevices\FlashCM40z.out
Fri Feb 25, 2022 15:32:35: Target reset
Fri Feb 25, 2022 15:32:35: Unloaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\config\flashloader\AnalogDevices\FlashCM40z.mac
Fri Feb 25, 2022 15:32:35: Downloaded E:\AnalogDevicenew20220223\AnalogDevice\ADSP-CM40x\CM403F_CM408F_EZ-KIT\examples\Button_LED_GPIO\CM408F\iar\Debug\Exe\Button_LED_GPIO.out to flash memory.
Fri Feb 25, 2022 15:32:35: 5001 bytes downloaded into FLASH (1.10 Kbytes/sec)
Fri Feb 25, 2022 15:32:36: IAR Embedded Workbench 8.32.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\bin\armproc.dll)