Post Go back to editing

Problems with CM408F on SPI protocol

I'm working with CM408F on SPI 0 but I have problem to read the answer of the connected slave, see timings below:

CH1: Is ChipSelect 
CH2: MISO
CH3: MOSI
CH4: SCLK
I send a command (0x38) on SPI to my slave and I must receive from it 0x2E88.
Scope dump confirm that sent and received data is correct.
But in my program I receive instead 012E88, and after this all rxed data is out of phase of one byte.
I can't find where my program is wrong or a patch to sync again data.
This is my init code (is a fragment):
unsigned baud;
bool cpha, cpol, msb;
volatile uint32_t * reg, wl;
reg = pREG_SPI0_CTL;
*pREG_PORTA_DATA_CLR = SPIENA;
*pREG_PORTA_DATA_CLR = PAD0 | PAD1 | PAD2 | PAD3; // Clear address
// Default values
REG_SPI_CTL = 0x00000010u;
REG_SPI_RXCTL = 0x00000000u;
REG_SPI_TXCTL = 0x00000000u;
REG_SPI_CLK = 0x00000000u;
REG_SPI_DLY = 0x00000301u;
REG_SPI_SLVSEL = 0x0000FE02u;
REG_SPI_RWC = 0x00000000u;
REG_SPI_RWCR = 0x00000000u;
REG_SPI_TWC = 0x00000000u;
REG_SPI_TWCR = 0x00000000u;

cpol = true;
cpha = false;
msb = true;
*pREG_PORTA_DATA_SET = PAD0 | PAD1 | PAD2; // Address = 7
baud = 1; // 2 MHz
wl = 8; // 8 bit

wl = wl / 8 - 1;
REG_SPI_CLK = PERIPHERALS_FREQUENCY / (baud + 1);
if(cpha) REG_SPI_CTL |= ENUM_SPI_CTL_SCKBEG;
if(cpol) REG_SPI_CTL |= ENUM_SPI_CTL_SCKLO;
if(!msb) REG_SPI_CTL |= ENUM_SPI_CTL_LSB_FIRST;
REG_SPI_CTL |= ((wl << BITP_SPI_CTL_SIZE) | ENUM_SPI_CTL_MASTER);
REG_SPI_RXCTL |= ENUM_SPI_RXCTL_RX_EN;
REG_SPI_TXCTL |= ENUM_SPI_TXCTL_TX_EN;
REG_SPI_CTL |= ENUM_SPI_CTL_EN;
*pREG_PORTA_DATA_SET = SPIENA;
REG_SPI_ICLR = BITM_SPI_ILAT_CLR_TF | BITM_SPI_ILAT_CLR_RF | BITM_SPI_ILAT_CLR_TS | BITM_SPI_ILAT_CLR_RS;

To send and receive data I use:

unsigned SpiSend(int spiNum, unsigned data)
{
volatile uint32_t * reg, d;
switch(spiNum)
{
case 0: reg = pREG_SPI0_CTL;
break;
case 1: reg = pREG_SPI1_CTL;
break;
case 2: reg = pREG_SPI2_CTL;
break;
}
REG_SPI_TX = data;
REG_SPI_RXCTL |= ENUM_SPI_RXCTL_RTI_EN;
REG_SPI_TXCTL |= ENUM_SPI_TXCTL_TTI_EN;
while(!(REG_SPI_STS & BITM_SPI_STAT_SPIF));
REG_SPI_TXCTL &= (~ENUM_SPI_TXCTL_TTI_EN);
REG_SPI_RXCTL &= (~ENUM_SPI_RXCTL_RTI_EN);
return REG_SPI_RX;
}

I hope someone can help me because I do not know what fish to catch!
Regards
Manuele