Article Can I use MATLAB/Simulink with the ADSP-CM40x?

Question

Can I use MATLAB and Simulink with the ADSP-CM40x and IAR Tool-chain?

==============================

Answer

While there is no direct interface between the IAR Tool-chain and MATLAB or Simulink, Mathworks offer the “Embedded Coder” product, an add-on which can generate portable C/C++ code from a MATLAB algorithm or Simulink model. The code generated from Embedded Coder can be compiled for the ADSP-CM40x processor using the IAR Tool-chain.

Embedded Coder further supports ARM by generating code that is optimized for ARM Cortex-M processors, such as the ADSP-CM40x. This ARM optimized code offers up to a significant execution performance improvement over ANSI/ISO C and supports MATLAB code, Simulink blocks, and DSP System Toolbox filters.

For more information, visit the Embedded Coder Product Page on the Mathworks website.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.