Post Go back to editing

WDT reset issue

Dear Team,

For your information, We are using ADSP21569 processor for our development.

Cross core studios 2.9.2 is used for development of the low level drivers and software, as per our standards we are planning to use direct read and writes to registers for code enhancement.

please provide information the below function which is used to clear all the pending interrupts at NVIC level.

Function name : ADI_WD_ACK_PENDINT()

The Below macro used in the code as a input parameter,

ADI_INT_WDOG0_EXP

Please do the needful on the same.

Regards,

Vignesh.

Parents
  • Hi Vignesh,

    Apologies for the delay. Were you able to get going. If you are still facing issue, please elaborate more about the issue.

    The ADI_WD_ACK_PENDINT acknowledges the pending interrupt at NVIC level. If the program is already running from Flash Watchdog interrupt gets invoked as soon as we install the handler.

    Regards,
    Anand Selvaraj.

Reply
  • Hi Vignesh,

    Apologies for the delay. Were you able to get going. If you are still facing issue, please elaborate more about the issue.

    The ADI_WD_ACK_PENDINT acknowledges the pending interrupt at NVIC level. If the program is already running from Flash Watchdog interrupt gets invoked as soon as we install the handler.

    Regards,
    Anand Selvaraj.

Children
No Data