Hello,
/SYS_FAULT is always asserted when power up (= /HWRST is negated ) the system using ADSP-21569.
What cause is considered about above situation?
The period of above /SYS_FAULT asserted is about 200ms.
Hello,
/SYS_FAULT is always asserted when power up (= /HWRST is negated ) the system using ADSP-21569.
What cause is considered about above situation?
The period of above /SYS_FAULT asserted is about 200ms.
Hi,
Apologies for delay in response.
1) Is the clock and voltage are within the specification of the ADSP-2156x datasheet?
www.analog.com/.../adsp-21562-21563-21565-21566-21567-21569.pdf
2) Is the /SYS_FAULT pin is always asserted for every power cycle/hard reset?
3) Did you follow the Power-Up Reset Timing, Is it possible to share the probing of the same?
Regards,
Anand Selvaraj.