Post Go back to editing

The clock synchronous issue for inputs & outputs signals of SHARC+ 2156x

Dear ADI engineers:

 Currently, when we designs an audio system with ADI SHARC+ DSP, we met a puzzled problem.  The basic system block is as below:

    Here, the audio source is driven by an A2B master(such as HU) by A2B_1 above. Besides that, we have another A2B (A2B_2 in the diagram above) for the data acquisition of MICs or other  signals, in which case SHARC+ act as the Host IC,A2B_2 as the A2B master and MICs act as the slave.
    As you see, the clock for A2B_1 is marked as red, which is provided by the master; while the clock for A2B_2 is marked as green, which is provided by SHARC+. To make the clock be synchronous between A2B_1 and A2B_2, the simple way is to use A2B_1’s clock to drive A2B_2’s clock inside SHARC+. But we don’t want to do as that, because it may make all the DSP audio processes (including A2B_2) depend too much on A2B_1, which will limit the extendibility and flexibility of our system.
     Another possible option for us is to use ASRC units inside SHARC+. But according to the chip specification, there are only 4 ASRC units for the input signals, which can make up a daisy-chain for the input TDM stream. And totally, we can process 8 TDM slots at most. And as you known, the input audio stream is with 16 TDM slots, which has exceeded the maximum ASRC capability. So it seems this solution is also infeasible.
   
      Since both A2B and SHARC+ are ADI products, we wish you can help us to give some suggestions.

Thanks!

Parents
  • Hi,

    1) Regarding,"Here, the audio source is driven by an A2B master(such as HU) by A2B_1 above. Besides that, we have another A2B (A2B_2 in the diagram above) for the data acquisition of MICs or other signals, in which case SHARC+ act as the Host IC,A2B_2 as the A2B master and MICs act as the slave. "
    >>   In A2B, By default Host will provide clock for A2B master,slave and slave connected peripherals. Once all the A2B connected Master and slave nodes are discovered.
    >>   All the A2B slave and A2B master are connected in line topology with Host. They are connected in daisy chain through a A2B cable(twisted pair).
    >>   Can you explain the setup? Which one is master here A2B_1 or A2B_2?
    >>   Are the A2B_1 and A2B_2 are individually interfaced with different ADSP-21565 SPORT channel like audio codec or is it connected with A2B bus?

    2) Regarding,"Here, the audio source is driven by an A2B master(such as HU) by A2B_1 above. Besides that, we have another A2B (A2B_2 in the diagram above) for the data acquisition of MICs or other signals,in which case SHARC+ act as the Host IC,A2B_2 as the A2B master and MICs act as the slave."
    >> Is ADSP-21565 is acting as a host or local processor connected to a Subordinate Node.

    3) Regarding,"To make the clock be synchronous between A2B_1 and A2B_2, the simple way is to use A2B_1’s clock to drive A2B_2’s clock inside SHARC+. But we don’t want to do as that, because it may make all the DSP audio processes (including A2B_2) depend too much on A2B_1, which will limit the extendibility and flexibility of our system."
    >> The Host provided bitclk and FS can be routed to ADSP-21565 using DAI SRU config and same clock can be used by A2B_2 also.

    4)  Regarding,"As you see, the clock for A2B_1 is marked as red, which is provided by the master;
    >>  How the master is getting bit clock and FS without Host?

    Regards,
    Anand Selvaraj.

  • Thanks Anand Selvaraj!
    [In A2B, By default Host will provide clock for A2B master,slave and slave connected peripherals. Once all the A2B connected Master and slave nodes are discovered.]
    ->Understood.

    [All the A2B slave and A2B master are connected in line topology with Host. They are connected in daisy chain through a A2B cable(twisted pair).]
    ->Understood

    [Can you explain the setup? Which one is master here A2B_1 or A2B_2?]
    -> Here, A2B_1 and A2B_2 are two different A2B daisy chain. For A2B_1, the host master maybe a HU, which should provide the bck & FS clock of A2B_1 chain. And for A2B_2, ADSP-21565 act as the host master, and MICs/sensors act as the slave.


    [Are the A2B_1 and A2B_2 are individually interfaced with different ADSP-21565 SPORT channel like audio codec or is it connected with A2B bus?]
    ->Yes, A2B_1 and A2B_2 are individually interfaced with different ADSP-21565 SPORT channel.

    [Is ADSP-21565 is acting as a host or local processor connected to a Subordinate Node.]
    ->For A2B_1, ADSP-21565 acts as a local processor connected to a Subordinate Node. For A2B_2, ADSP-21565 acts as a host master.

    [The Host provided bitclk and FS can be routed to ADSP-21565 using DAI SRU config and same clock can be used by A2B_2 also.]
    -> Yes, this is the same as what we do now. But I think it will limit the extendibility and flexibility of our system. So I want to know if there is any better solutions/designs for the system.

    [How the master is getting bit clock and FS without Host?]
    ->For A2B_1, the host master maybe a HU which is missed out in the diagram. The HU should locate at the left side in the block. For A2B_2, the host master is ADSP-21565. its BCK & FS should be provided either by ADSP-21565 internal clock or by the external clock(from A2B_1). We wish it should be provided by ADSP-21565 internal clock. But we don't know how to solve the clock synchronous issue between A2B_1 and A2B_2.

  • Hi,

    1) Regarding,"Yes, this is the same as what we do now. But I think it will limit the extendibility and flexibility of our system. So I want to know if there is any better solutions/designs for the system."
    >> Are you getting any issues?
    >> Are the A2B_1 and A2B_2 working at different frame sync rates?

    2)Regarding,"For A2B_1, the host master maybe a HU which is missed out in the diagram. The HU should locate at the left side in the block. For A2B_2, the host master is ADSP-21565. its BCK & FS should be provided either by ADSP-21565 internal clock or by the external clock(from A2B_1). We wish it should be provided by ADSP-21565 internal clock. But we don't know how to solve the clock synchronous issue between A2B_1 and A2B_2."
    >>If A2B_1 and A2B_2 both are working individually(not connected through A2B bus daisy chain) or A2B_1 master is not controlling(no upstream/downstream communication between A2B_1 and A2B_2) A2B_2 slave, then
      Can you try with PCG from ADSP-21565 to A2B_2?

    Regards,
    Anand Selvaraj.

Reply
  • Hi,

    1) Regarding,"Yes, this is the same as what we do now. But I think it will limit the extendibility and flexibility of our system. So I want to know if there is any better solutions/designs for the system."
    >> Are you getting any issues?
    >> Are the A2B_1 and A2B_2 working at different frame sync rates?

    2)Regarding,"For A2B_1, the host master maybe a HU which is missed out in the diagram. The HU should locate at the left side in the block. For A2B_2, the host master is ADSP-21565. its BCK & FS should be provided either by ADSP-21565 internal clock or by the external clock(from A2B_1). We wish it should be provided by ADSP-21565 internal clock. But we don't know how to solve the clock synchronous issue between A2B_1 and A2B_2."
    >>If A2B_1 and A2B_2 both are working individually(not connected through A2B bus daisy chain) or A2B_1 master is not controlling(no upstream/downstream communication between A2B_1 and A2B_2) A2B_2 slave, then
      Can you try with PCG from ADSP-21565 to A2B_2?

    Regards,
    Anand Selvaraj.

Children
No Data