What DCLK speed is supported for ADP-2156x BGA variant processor from Sil revision 0.0 to 0.2?

What DCLK speed is supported for ADP-2156x BGA variant processor from Sil revision 0.0 to 0.2?

  • 0
    •  Analog Employees 
    on Sep 14, 2020 7:42 AM 2 months ago

    In Silicon revision 0.0, the maximum DCLK supported is 500MHz. This silicon revision can be used for consumer use cases.

     

    In the silicon revision 0.2,

    • Maximum DCLK supported is 667MHz for all automotive/consumer and industrial use cases.
    • For CCLK of 1GHz, the DCLK of 500MHz, is only supported for temperature above 0°C as mentioned in the latest datasheet.

     

    There is no change in terms of the hardware when migrating from silicon revision 0.0 to 0.2.