CGUPowerServiceConfig_21569 Example - How to Configure?

This example contains two files adi_pwr_config0.c and adi_pwr_config1.c which contain the comment

** This file is generated automatically based upon the options selected in
** the Basic Configuration of CGU Initialization configuration dialog. Changes to this configuration should be made by
** changing the appropriate options rather than editing this file.

But where do I set these options?  Where is the Basic Configuration of CGU Initialization configuration dialog?  How do I generate these files?

Thanks,

Matt

Parents
  • 0
    •  Analog Employees 
    on Feb 24, 2021 10:28 AM

    Hi,

    Sorry for the delayed response.

    Please note that, In future, a GUI will be provided for all relevant modules so that user do not have to modify the static configuration header files manually. After user configure the peripheral's parameter using GUI, it will generate the static configuration header file and add it to the application project.

    We suggest you to refer the 3.3 Static Configuration of Peripherals (PageNo:6/14) section in the SystemServices_and_DeviceDrivers_UserGuide. You can get this PDF from the below installation path:
    C:\Analog Devices\CrossCore Embedded Studio 2.9.3\Docs

    Regards,
    Anand Selvaraj.

Reply
  • 0
    •  Analog Employees 
    on Feb 24, 2021 10:28 AM

    Hi,

    Sorry for the delayed response.

    Please note that, In future, a GUI will be provided for all relevant modules so that user do not have to modify the static configuration header files manually. After user configure the peripheral's parameter using GUI, it will generate the static configuration header file and add it to the application project.

    We suggest you to refer the 3.3 Static Configuration of Peripherals (PageNo:6/14) section in the SystemServices_and_DeviceDrivers_UserGuide. You can get this PDF from the below installation path:
    C:\Analog Devices\CrossCore Embedded Studio 2.9.3\Docs

    Regards,
    Anand Selvaraj.

Children
No Data