Generate an application LDR with schematic code and parameter embedded in it or ADSP-2156x

Hi all,

I would like to know if there is a way to generate an application LDR with a schematic code and parameter embedded in it?

I found for ADSP-214xx series a post here

"https://ez.analog.com/dsp/software-and-development-tools/sigmastudio-for-sharc/w/documents/9487/faq-is-it-possible-to-generate-an-application-ldr-with-schematic-code-and-parameter-embedded-in-it"

which explains how to proceed but unfortunately it's just compliant with SigmaStudio for SHARC 2.2.0.

I am using SigmaStudio for SHARC 4.5.0 and CrossCore 2.9.2. The purpose is to create an LDR with a schematic code and parameter embedded in it dedicated to ADSP-2156x.

All the raw code will be inside a "C" tab within a header ".h" file.

Example:

const unsigned char sS_LDR[LDR_SIZE] = {
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
...,..,..
}

Thus, I will load the entire program inside the DSP at the system's start-up sequence.

Let le know if you need further details,

Please advise, 

Thank you,

Regards