What enhancements have been done in ADSP-2156x FIR/IIR accelerators?

What enhancements have been done in ADSP-2156x FIR/IIR accelerators?

  • +1
    •  Analog Employees 
    on Sep 5, 2019 9:26 AM over 1 year ago

    The following are the enhancements made in ADSP-2156x FIR/IIR accelerators:

    Performance Improvements: 

    - The operating frequency is increased to 1 GHz (=CCLK) as compared to 125/112.5 MHz (=SCLK) on ADSP_2157x.

    - The Data and MMR latency is reduced with closer integration of SHARC Core and Accelerators.

    Functional Improvements:

    - Additional Mode known as Auto Configuration mode is supported along with legacy mode.

    - It allows FIRCTL1 register to be loaded from TCB

    - No Channel Number limitation

    - Halt feature which allows for smart task queuing

    - Trigger generation(Master) and trigger wait(slave) to allow event sequencing.