[#5730] u-boot can not boot on bf533 board

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#5730] u-boot can not boot on bf533 board

Submitted By: Vivi Li

Open Date

2009-11-30 22:34:45     Close Date

2009-12-01 22:53:37

Priority:

Medium     Assignee:

Mike Frysinger

Category:

N/A     Fixed In Release:

2010R1

Found In Release:

2010R1     Status:

Closed

Board:

N/A     Processor:

BF533

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: u-boot can not boot on bf533 board

Details:

 

u-boot can not boot on bf533-stamp/bf533-ezkit since Nov 16th.

 

Bellow I tried the latest u-boot.bin on bf533-stamp.

--

U-Boot 2009.08-svn2083 (ADI-2009R2-pre) (Nov 16 2009 - 14:59:48)

 

CPU:   ADSP bf533-0.3 (Detected Rev: 0.3) (bypass boot)

Board: ADI BF533 Stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 497.664 MHz, Core: 497.664 MHz, System: 82.944 MHz

RAM:   128 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   SMC91111-0

Warning: SMC91111-0 MAC addresses don't match:

Address in SROM is         ba:5f:37:c8:87:b3

Address in environment is  00:e0:22:fe:36:54

 

Hit any key to stop autoboot:  0

bfin>

bfin> tftp 0x1000000 u-boot.bin

SMC91111: MAC 00:e0:22:fe:36:54

Using SMC91111-0 device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'u-boot.bin'.

Load address: 0x1000000

Loading: ############

done

Bytes transferred = 168384 (291c0 hex)

bfin> go 0x1000000

## Starting application at 0x01000000 ...

 

--

 

Follow-ups

 

--- Mike Frysinger                                           2009-12-01 17:00:19

git bisect says commit r2095 is to blame (Blackfin: use new bfin read/write mmr

helper funcs)

 

--- Mike Frysinger                                           2009-12-01 17:28:22

looks like i typoed the uart base address for devices that only have 1 uart

 

--- Vivi Li                                                  2009-12-01 22:53:37

OK now.

Close it.

 

--- Vadim Galitsyn                                           2011-02-05 12:14:00

This issue is still reproducible on bf533-stamp rev. 1.1 with

u-boot-2010.06-2010R1-RC2. I tried to apply the patch available by:

 

svn diff

svn://sources.blackfin.uclinux.org/u-boot/trunk/u-boot-2009.08/cpu/blackfin/serial.h@2114

svn://sources.blackfin.uclinux.org/u-boot/trunk/u-boot-2009.08/cpu/blackfin/serial.h@2113

 

but, it does not help.

 

================================================

U-Boot-1.1.3-ADI-2005R4 (Feb 19 2006 - 15:23:29)

 

CPU:   ADSP BF533 Rev.: 0.3

Board: ADI BF533 Stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 398 MHz, Core: 398 MHz, System: 79 MHz

SDRAM: 128 MB

FLASH:   4 MB

In:    serial

Out:   serial

Err:   serial

Net:   SMC91111 at 0x20300300

I2C:   ready

Hit any key to stop autoboot:  0

stamp>

stamp>

stamp>

stamp>dhcp

Using MAC Address 00:E0:22:FE:03:F2

BOOTP broadcast 1

DHCP client bound to address 192.168.0.5

stamp>tftp 0x1000000 u-boot.bin

Using MAC Address 00:E0:22:FE:03:F2

TFTP from server 192.168.0.1; our IP address is 192.168.0.5

Filename 'u-boot.bin'.

Load address: 0x1000000

Loading: ###################################

done

Bytes transferred = 178624 (2b9c0 hex)

stamp>go 0x1000000

## Starting application at 0x01000000 ...

 

--- Vadim Galitsyn                                           2011-02-05 12:16:07

I also tried to boot

http://blackfin.uclinux.org/gf/download/frsrelease/499/8439/u-boot-bf533-stamp-2010R1-RC2.tar.bz2

images. The result was the same.

 

--- Mike Frysinger                                           2011-02-05 12:43:26

your issue is unrelated.  please post your question to the forums.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes