[#5471] MAC address should be in capital in u-boot boot message

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#5471] MAC address should be in capital in u-boot boot message

Submitted By: Vivi Li

Open Date

2009-08-30 22:10:11     Close Date

2009-08-31 00:09:21

Priority:

Medium     Assignee:

Mike Frysinger

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

N/A     Processor:

BF518

Silicon Revision:

    Resolution:

Rejected

Is the bug repeatable?:

N/A     

Summary: MAC address should be in capital in u-boot boot message

Details:

 

The MAC address showing up in u-boot boot message on bf517f-ezbrd is in lower case, while it's in capital for other platform.

 

Bellow is the log:

--

U-Boot 2009.06-svn2013 (ADI-2009R2-pre) (Aug 30 2009 - 08:39:35)

 

CPU:   ADSP bf518-0.0 (Detected Rev: 0.0) (parallel flash boot)

Board: ADI BF518F EZ-Board board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 625 MHz, Core: 156.250 MHz, System: 78.125 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   00:e0:22:fe:55:b3

Hit any key to stop autoboot:  0

bfin> printenv

bootargs=root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600

baudrate=57600

loads_echo=1

autoload=no

rootpath=/romfs

hostname=bf518f-ezbrd

loadaddr=0x1000000

ubootfile=u-boot.ldr

update=tftp $(loadaddr) $(ubootfile);protect off 0x20000000 +$(filesize);erase 0x20000000 +$(filesize);cp.b $(loadaddr) 0x200000)

addip=set bootargs $(bootargs) ip=$(ipaddr):$(serverip):$(gatewayip):$(netmask):$(hostname):eth0:off

ramfile=uImage

ramargs=set bootargs root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600

ramboot=tftp $(loadaddr) $(ramfile);run ramargs;run addip;bootm

nfsfile=vmImage

nfsargs=set bootargs root=/dev/nfs rw nfsroot=$(serverip):$(rootpath),tcp,nfsvers=3

nfsboot=tftp $(loadaddr) $(nfsfile);run nfsargs;run addip;bootm

flashboot=bootm 0x20100000

ethact=Blackfin EMAC

tftp_boot=tftp 0x1000000 linux.dxe;boote 0x1000000

bootdelay=9

date_tested=Sun Aug 30 10:37:27 GMT-8 2009

filesize=170C81

fileaddr=1000000

gatewayip=10.100.4.174

netmask=255.255.255.0

ipaddr=10.100.4.50

serverip=10.100.4.174

bootcmd=bootm 0x20100000

ethaddr=00:E0:22:FE:55:B3

stdin=serial

stdout=serial

stderr=serial

 

Environment size: 1186/8188 bytes

bfin>

--

 

Follow-ups

 

--- Mike Frysinger                                           2009-08-31 04:16:35

mmm i doubt it.  it's common code that shows the MAC and it does it the same

way.  perhaps it has changed between versions, but at any rate, whether it's

lower or upper doesnt matter.

 

--- Vivi Li                                                  2009-08-31 05:10:21

Yeah, I made some mistake.

All the platform are in lower case now and in 09r1 release they are all in

capital letters. That's the version difference.

So close this bug.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes