[#5289] soft reset fails to execute on BF526 after cp.b operation

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#5289] soft reset fails to execute on BF526 after cp.b operation

Submitted By: Vivi Li

Open Date

2009-06-22 05:09:50     Close Date

2009-06-22 08:57:22

Priority:

Medium High     Assignee:

Mike Frysinger

Category:

N/A     Fixed In Release:

N/A

Found In Release:

2009R1     Status:

Closed

Board:

N/A     Processor:

BF526

Silicon Revision:

    Resolution:

Duplicated

Is the bug repeatable?:

N/A     

Summary: soft reset fails to execute on BF526 after cp.b operation

Details:

 

After cp.b operation, soft reset fails to execute on BF526-EZBRD.

 

Bellow is the log:

--

U-Boot 2008.10-svn1905 (ADI-2009R1-rc1) (Jun 10 2009 - 11:20:25)

 

CPU:   ADSP bf526-0.0 (Detected Rev: 0.0) (parallel flash boot)

Board: ADI BF526 EZ-Board board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 80 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   B2:63:4D:0F:0A:77

Hit any key to stop autoboot:  0

bfin>

bfin> tftpboot 0x1000000 uImage

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         ##################

done

Bytes transferred = 4074510 (3e2c0e hex)

bfin> tftpboot 0x1000000 u-boot.bin

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'u-boot.bin'.

Load address: 0x1000000

Loading: ############

done

Bytes transferred = 175540 (2adb4 hex)

bfin> protect off 0x20080000 0x203fffff

........................................................ done

Un-Protected 56 sectors

bfin> erase 0x20080000 0x203fffff

 

........................................................ done

Erased 56 sectors

bfin> cp.b 0x1000000 0x20080000 0x2adb4

Copy to Flash... done

bfin> reset

(can not boot up now, need hardware reset)

--

 

--

U-Boot 2008.10-svn1905 (ADI-2009R1-rc1) (Jun 10 2009 - 11:20:25)

 

CPU:   ADSP bf526-0.0 (Detected Rev: 0.0) (parallel flash boot)

Board: ADI BF526 EZ-Board board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 80 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   B2:63:4D:0F:0A:77

Hit any key to stop autoboot:  0

bfin>

bfin> protect off all

Un-Protect Flash Bank # 1

....................................................................... done

bfin> cp.b 0x1000000 0x20390000 0x200

Copy to Flash... done

bfin> reset

(can not boot up now, need hardware reset)

--

 

Follow-ups

 

--- Mike Frysinger                                           2009-06-22 08:57:22

pretty sure this is a duplicate of [#4884]

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes