[#5124] MUSB is broken in u-boot-2009.03+

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#5124] MUSB is broken in u-boot-2009.03+

Submitted By: Mike Frysinger

Open Date

2009-05-13 19:56:04     Close Date

2009-12-29 04:42:12

Priority:

Medium     Assignee:

Cliff Cai

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

N/A     Processor:

BF548

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: MUSB is broken in u-boot-2009.03+

Details:

 

the musb version that was originally merged in 2008.10 was rewritten more upstream before being merged.  i tried forward porting things (instead of using register define offsets, it uses a struct now), but it doesnt seem to work properly.

 

Follow-ups

 

--- Sonic Zhang                                              2009-05-14 00:00:20

Cliff took over the USB bugs.

 

--- Vivi Li                                                  2009-08-27 02:34:14

usb can not work in trunk.

 

--

U-Boot 2009.06-svn2006 (ADI-2009R2-pre) (Aug 27 2009 - 04:21:53)

 

CPU:   ADSP bf527-0.0 (Detected Rev: 0.2) (parallel flash boot)

Board: ADI BF527 EZ-Kit board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 100 MHz, System: 50 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   00:e0:22:fe:bf:34

Hit any key to stop autoboot:  0

bfin>

bfin> usb start

(Re)start USB...

USB:   scanning bus for devices... No USB Device found

       scanning bus for storage devices... 0 Storage Device(s) found

bfin>

--

 

--- Cliff Cai                                                2009-11-11 04:53:34

fixed by correcting some errors caused by upstream.

 

--- Vivi Li                                                  2009-12-29 04:42:17

Test pass for u-boot-2009.08.

Close this bug

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes