[#4979] bf518 spi uboot on svn trunk 2008.10 fails to boot after kernel reboots

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#4979] bf518 spi uboot on svn trunk 2008.10 fails to boot after kernel reboots

Submitted By: Sonic Zhang

Open Date

2009-03-11 06:29:33     Close Date

2010-01-14 02:19:03

Priority:

Medium High     Assignee:

Sonic Zhang

Category:

N/A     Fixed In Release:

N/A

Found In Release:

2009R1     Status:

Closed

Board:

Ezbrd     Processor:

BF518

Silicon Revision:

0.0     Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: bf518 spi uboot on svn trunk 2008.10 fails to boot after kernel reboots

Details:

 

bf518 spi uboot fails to boot after kernel reboots.

toolchain rev. 09R1-RC2

uboot svn trunk 2008.10

 

 

U-Boot 2008.10-svn1698 (ADI-2009R1-pre) (Mar 11 2009 - 17:48:59)

 

CPU:   ADSP bf518-0.0 (Detected Rev: 0.0) (spi flash boot)

Board: ADI BF518F EZ-Board board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 80 MHz

RAM:   64 MB

Flash:  4 MB

SF: Got idcode 20 20 15

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   86:84:83:DD:38:24

Hit any key to stop autoboot:  0                                                          

 

 

BusyBox v1.13.2 (2009-03-11 18:06:30 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/>

root:/>

root:/>

root:/> reboot

Restarting system.

 

Follow-ups

 

--- Sonic Zhang                                              2009-03-18 05:30:35

wait for feedback from hardware designer to figure out how to deal with the

kernel reboot workaround.

 

--- Sonic Zhang                                              2009-04-01 05:21:25

work around in kernel.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes