[#4889] In BF548 u-boot, no Fat file system in hard disk is detected

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#4889] In BF548 u-boot, no Fat file system in hard disk is detected

Submitted By: Vivi Li

Open Date

2009-02-11 03:02:06     Close Date

2009-02-12 02:49:00

Priority:

Medium     Assignee:

Nobody

Category:

N/A     Fixed In Release:

N/A

Found In Release:

2009R1     Status:

Closed

Board:

N/A     Processor:

N/A

Silicon Revision:

    Resolution:

Rejected

Is the bug repeatable?:

N/A     

Summary: In BF548 u-boot, no Fat file system in hard disk is detected

Details:

 

In BF548 u-boot, no Fat file system in hard disk is detected.

This fs is created in kernel and can be detected in kernel.

 

--

U-Boot 2008.10-svn1666 (ADI-2009R1-pre) (Feb 11 2009 - 10:34:47)

 

CPU:   ADSP bf548-0.0 (Detected Rev: 0.1) (parallel flash boot)

Board: ADI BF548 EZ-Kit board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131.250 MHz

RAM:   64 MB

Flash: 16 MB

NAND:  256 MiB

In:    serial

Out:   serial

Err:   serial

Net:   MAC:   00:E0:22:FE:B8:3D

Hit any key to stop autoboot:  0

bfin>

bfin> sata init

PATA device#0 TOSHIBA MK4032GAX is found on ata port#0.

bfin> fatls sata 0

No Fat FS detected

bfin> fatinfo sata 0

Interface:  SATA

  Device 0: Model: TOSHIBA MK4032GAX Firm: AD101A Ser#:            97P9TBG6T

            Type: Hard Disk

            Supports 48-bit addressing

            Capacity: 38154.3 MB = 37.2 GB (78140160 x 512)

 

No valid FAT fs found

bfin>

bfin>

bfin> tftp 0x1000000 uImage.sdiommc

smc911x: initializing

smc911x: detected LAN9218 controller

smc911x: phy initialized

smc911x: MAC 00:e0:22:fe:b8:3d

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage.sdiommc'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ###############################################

done

Bytes transferred = 5451670 (532f96 hex)

bfin> bootm

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   Linux-2.6.28.3-ADI-2009R1-pre-sv

   Created:      2009-02-10  10:53:53 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    5451606 Bytes =  5.2 MB

   Load Address: 00001000

   Entry Point:  0028d5cc

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 0028d5cc

Linux version 2.6.28.3-ADI-2009R1-pre-svn6083 (test@uclinux61-bf548-std) (gcc version 4.1.2 (ADI sv9

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001b9770

  rodata    = 0x001b9770-0x0024e61c

  bss       = 0x0024e620-0x0026070c

  data      = 0x0026070c-0x00278000

    stack   = 0x00276000-0x00278000

  init      = 0x00278000-0x00a1e000

  available = 0x00a1e000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF548 Rev 0.1

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15747

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 consol0

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 52544k/65536k RAM, (7832k init code, 1761k kernel code, 763k data, 2048k dma, 584)

Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

Blackfin L2 SRAM: 128 KB (128 KB free)

PDA for CPU0 reserved at 0024fed8

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

 

 

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, musb-dma, host, debug=0

musb_hdrc: USB Host mode controller at ffc03c00 using DMA, IRQ 82

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

dma_alloc_init: dma_page @ 0x03dde000 - 512 pages at 0x03e00000

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 102

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bf54x-lq043: FrameBuffer initializing...

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 48) is a BFIN-UART

brd: module loaded

smsc911x: Driver version 2007-07-13.

eth0: SMSC911x MAC Address: 00:e0:22:fe:b8:3d

Driver 'sd' needs updating - please use bus_type methods

Driver 'sr' needs updating - please use bus_type methods

register bfin atapi driver

scsi0 : pata-bf54x

ata1: PATA max UDMA/66 irq 68

ata1.00: ATA-6: TOSHIBA MK4032GAX, AD101A, max UDMA/100

ata1.00: 78140160 sectors, multi 16: LBA48

ata1.00: configured for UDMA/66

blk_queue_max_hw_segments: set to minimum 1

scsi 0:0:0:0: Direct-Access     ATA      TOSHIBA MK4032GA AD10 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 78140160 512-byte hardware sectors: (40.0 GB/37.2 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sd 0:0:0:0: [sda] 78140160 512-byte hardware sectors: (40.0 GB/37.2 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sda: sda1 sda2

sd 0:0:0:0: [sda] Attached SCSI disk

physmap platform flash device: 02000000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Using buffer write method

Using auto-unlock on power-up/resume

cfi_cmdset_0001: Erase suspend on write enabled

RedBoot partition parsing not available

Using physmap partition information

Creating 3 MTD partitions on "physmap-flash.0":

0x00000000-0x00040000 : "bootloader(nor)"

0x00040000-0x00440000 : "linux kernel(nor)"

0x00440000-0x01000000 : "file system(nor)"

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader(spi)"

0x00040000-0x00200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma c4

bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc02300, dma c5

input: bf54x-keys as /devices/platform/bf54x-keys/input/input0

bf54x-keys: Blackfin BF54x Keypad registered IRQ 76

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc00700

i2c-bfin-twi i2c-bfin-twi.1: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc02200

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

hid_tmff: Unknown symbol _input_ff_create_memless

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

mmc0: new SD card at address 80ca

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

ASoC version 0.13.2

mmcblk0: mmc0:80ca SD256 241 MiB

mmcblk0:<3>dma rx:0 tx:1, err irq:10, regs:ffc00800

AD1980 SoC Audio Codec

asoc: AC97 <-> bf5xx-ac97 mapping ok

p1

ALSA device list:

  #0: bf5xx-board (AD1980)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2003-02-14 11:19:19 UTC (1045221559)

Freeing unused kernel memory: 7832k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.2 (2009-02-10 10:30:54 GMT) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> mount /dev/mmusb 1-1: new high speed USB device using musb_hdrc and address 2

usb 1-1: configuration #1 chosen from 1 choice

root:/> mount /dev/mmcblk0p1 /mnt/

root:/> mount

rootfs on / type rootfs (rw)

proc on /proc type proc (rw,nosuid,nodev,noexec)

sysfs on /sys type sysfs (rw,nosuid,nodev,noexec)

mdev on /dev type tmpfs (rw,nosuid)

devpts on /dev/pts type devpts (rw,nosuid,noexec,mode=600)

var on /var type ramfs (rw)

tmp on /tmp type tmpfs (rw,nosuid,nodev)

debugfs on /sys/kernel/debug type debugfs (rw)

/dev/mmcblk0p1 on /mnt type vfat (rw,fmask=0022,dmask=0022,codepage=cp850,iocharset=iso8859-1)

root:/> ls /mnt/

uImage

root:/>

--

 

Follow-ups

 

--- Mike Frysinger                                           2009-02-11 11:39:02

you mounted the sd card under Linux, not the hard drive

 

--- Vivi Li                                                  2009-02-12 02:49:00

Stupid mistake... I was testing both mmc and sata at that time...

So close it. Thanks!

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes