[#4840] u-boot requires ldr with -J and --bmode flags to --create

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#4840] u-boot requires ldr with -J and --bmode flags to --create

Submitted By: Tom Parker

Open Date

2009-01-23 09:19:04     Close Date

2009-02-23 17:33:20

Priority:

Medium High     Assignee:

Nobody

Category:

Make     Fixed In Release:

N/A

Found In Release:

snaps     Status:

Closed

Board:

Custom     Processor:

BF537

Silicon Revision:

    Resolution:

Rejected

Is the bug repeatable?:

yes     

Summary: u-boot requires ldr with -J and --bmode flags to --create

Details:

 

u-boot requires a version of ldr with -J and --bmode flags to --create or the build fails, and they're only present in fairly recent versions of ldr-utils (which we don't have installed). However, if these flags are removed, u-boot builds properly, and so u-boot should be changed to only use these flags if available.

 

I've attached a patch to fix this against current SVN HEAD of the u-boot-2008.10 directory, but it should probably also work with the 2009 stuff as well.

 

Follow-ups

 

--- Mike Frysinger                                           2009-01-23 09:59:56

trunk u-boot requires trunk toolchain.  grab a toolchain snapshot if you want to

use it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

check-for-flags.patch    text/x-diff    659    Tom Parker

Attachments

Outcomes