[#4668] asm/arch doesn't point to mach-bf548 when configure u-boot-2008.10 for bf548-ezkit

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#4668] asm/arch doesn't point to mach-bf548 when configure u-boot-2008.10 for bf548-ezkit

Submitted By: Cliff Cai

Open Date

2008-11-25 04:28:45     Close Date

2008-12-06 02:47:25

Priority:

Medium High     Assignee:

Mike Frysinger

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

EZ-Kit Lite     Processor:

N/A

Silicon Revision:

    Resolution:

Rejected

Is the bug repeatable?:

yes     

Summary: asm/arch doesn't point to mach-bf548 when configure u-boot-2008.10 for bf548-ezkit

Details:

 

make bf548-ezkit_config

ls -l include/asm/arch

shows that: include/asm/arch -> arch-blackfin

it should be linked to mach-bf548

 

Cliff

 

Follow-ups

 

--- Mike Frysinger                                           2008-11-25 12:27:47

we dont use asm/arch/ and we shouldnt be

 

--- Cliff Cai                                                2008-11-25 22:03:59

but a common file:include/mmc.h needs to include a file:asm/arch/mmc.h for

SD/MMC

driver.

 

Cliff

 

--- Mike Frysinger                                           2008-11-26 02:37:37

the current common sdio design sucks.  this is why i suggested we wait for the

nice rewrite that's going on with mainline atm.  but we have the driver done

now, so i'll just hack the common sdio code to not rely on arch-specific paths.

after all the current common code is getting completely tossed in one the next

versions of u-boot.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes