[#4606] there is no response when tftp download or ping in bf537-stamp u-boot 2008.10

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#4606] there is no response when tftp download or ping in bf537-stamp u-boot 2008.10

Submitted By: Vivi Li

Open Date

2008-11-04 23:16:10     Close Date

2008-11-05 21:33:37

Priority:

Medium     Assignee:

Mike Frysinger

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

N/A     Processor:

N/A

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: there is no response when tftp download or ping in bf537-stamp u-boot 2008.10

Details:

 

It hangs when tftp download or ping in bf537-stamp u-boot 2008.10.

 

Bellow is the log when download a image in 537:

--

U-Boot 2008.10-svn1458 (ADI-2009R1-pre) (Nov  5 2008 - 12:26:28)

 

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 100 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Warning: Generating 'random' MAC address

Blackfin EMAC

MAC:   82:82:8B:2D:3D:18

Hit any key to stop autoboot:  0

bfin>

bfin> print

bootargs=root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 console=ttyBF0,57600

bootcmd=run ramboot

bootdelay=5

baudrate=57600

loads_echo=1

ipaddr=192.168.0.15

serverip=192.168.0.2

autoload=no

rootpath=/romfs

gatewayip=192.168.0.1

netmask=255.255.255.0

hostname=bf537-stamp

loadaddr=0x1000000

ubootfile=u-boot.bin

update=tftp $(loadaddr) $(ubootfile);protect off 0x20000000 0x2003FFFF;erase 0x20000000 0x2003FFFF;cp.b $(loadaddr) 0x20000000 )

addip=set bootargs $(bootargs) ip=$(ipaddr):$(serverip):$(gatewayip):$(netmask):$(hostname):eth0:off

ramargs=set bootargs root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 console=ttyBF0,57600

ramboot=tftp $(loadaddr) uImage;run ramargs;run addip;bootm

nfsargs=set bootargs root=/dev/nfs rw nfsroot=$(serverip):$(rootpath),tcp,nfsvers=3

nfsboot=tftp $(loadaddr) vmImage;run nfsargs;run addip;bootm

flashboot=bootm 0x20100000

stdin=serial

stdout=serial

stderr=serial

ethact=Blackfin EMAC

ethaddr=82:82:8B:2D:3D:18

 

Environment size: 974/8188 bytes

bfin> set ipaddr 10.100.4.50

bfin> set serverip 10.100.4.174

bfin> tftp 0x1000000 u-boot.bin

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'u-boot.bin'.

Load address: 0x1000000

Loading: *

(no response to Ctrl+C)

--

 

Follow-ups

 

--- Mike Frysinger                                           2008-11-05 07:24:41

should be fixed now

 

--- Vivi Li                                                  2008-11-05 21:33:37

OK now. Close it. Thanks!

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes