[#4403] trunk u-boot for bf533 stamp can't do reset

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#4403] trunk u-boot for bf533 stamp can't do reset

Submitted By: Mingquan Pan

Open Date

2008-09-02 23:02:39     Close Date

2008-09-08 01:17:00

Priority:

Medium     Assignee:

Mike Frysinger

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

N/A     Processor:

N/A

Silicon Revision:

    Resolution:

Duplicated

Is the bug repeatable?:

N/A     

Summary: trunk u-boot for bf533 stamp can't do reset

Details:

 

trunk u-boot for bf533 stamp can't do reset.

 

U-Boot 1.1.6-svn1337 (ADI-2009R1-pre) (Sep  2 2008 - 15:04:59)

 

CPU:   ADSP bf533-0.3 (Detected Rev: 0.3)

Board: ADI BF533 Stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 398 MHz, Core: 398 MHz, System: 79 MHz

RAM:   128 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   SMC91111 at 0x20300300

MAC:   00:E0:22:FE:07:5B

Hit any key to stop autoboot:  0

bfin> print

bootcmd=run ramboot

baudrate=57600

loads_echo=1

autoload=no

rootpath=/checkout/uClinux-dist/romfs

hostname=1

loadaddr=0x1000000

ubootfile=u-boot.bin

update=tftp $(loadaddr) $(ubootfile);protect off 0x20000000 0x2003FFFF;erase 0x20000000 0x2003FFFF;cp.b $(loadaddr) 0x20000000 $(filesize)

addip=set bootargs $(bootargs) ip=$(ipaddr):$(serverip):$(gatewayip):$(netmask):$(hostname):eth0:off

ramargs=set bootargs root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

nfsargs=set bootargs root=/dev/nfs rw nfsroot=$(serverip):$(rootpath),tcp,nfsvers=3

nfsboot=tftp $(loadaddr) vmImage;run nfsargs;run addip;bootm

flashboot=bootm 0x20100000

ethaddr=00:E0:22:FE:07:5B

ramboot=tftp $(loadaddr) linux;run ramargs;run addip;boote

bootdelay=5

bootargs=root=mtd0 rootfstype=romfs ro

filesize=23694

fileaddr=1000000

gatewayip=10.100.4.174

netmask=255.255.255.0

ipaddr=10.100.4.50

serverip=10.100.4.174

stdin=serial

stdout=serial

stderr=serial

 

Environment size: 931/8188 bytes

bfin> reset

 

Stucks here.

 

And it was first found on u-boot of Aug 13.

 

U-Boot 1.1.6-svn1322 (ADI-2008R2-pre) (Aug 13 2008 - 18:44:56)^M

^M

CPU:   ADSP bf533-0.3 (Detected Rev: 0.3)^M

Board: ADI BF533 Stamp board^M

       Support: http://blackfin.uclinux.org/^M

Clock: VCO: 398 MHz, Core: 398 MHz, System: 79 MHz^M

RAM:   128 MB^M

Flash:  4 MB^M

In:    serial^M

Out:   serial^M

Err:   serial^M

Net:   SMC91111 at 0x20300300^M

MAC:   BA:5F:37:C8:87:B3^M

Hit any key to stop autoboot:  9 ^H^H^H 0 ^M

bfin> Recovered to the u-boot prompt

waiting for uboot prompt

Attempting to recover to u-boot prompt

<INTERRUPT>^M

...bfin> got u-boot prompt

icache on^M

Instruction Cache is ON^M

bfin> dcache on^M

Data (writethrough) Cache is ON^M

bfin> reset^M

ERROR: u-boot got lost during reset command

ERROR: u-boot got lost during reset command

 

 

 

Follow-ups

 

--- Mike Frysinger                                           2008-09-08 01:16:58

dupe of [#4342]

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes