[#4177] run mtest only in 08r1 branch u-boot would have fail on bf548

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#4177] run mtest only in 08r1 branch u-boot would have fail on bf548

Submitted By: Mingquan Pan

Open Date

2008-06-19 00:17:22     Close Date

2008-06-26 05:46:00

Priority:

Medium     Assignee:

Mike Frysinger

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

N/A     Processor:

N/A

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: run mtest only in 08r1 branch u-boot would have fail on bf548

Details:

 

run mtest only in 08r1 branch u-boot would have fail on bf548.

 

If give the detailed address, it could run ok.

 

U-Boot 1.1.6-svn1147 (ADI-2008R1) (Feb 18 2008 - 15:51:24)

 

CPU:   ADSP bf548-0.0 (Detected Rev: 0.0)

Board: ADI BF548 EZ-Kit board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131 MHz

RAM:   64 MB

Flash: 32 MB

In:    serial

Out:   serial

Err:   serial

NAND:  256 MiB

Net:   LAN9x18 (0x118a0000) detected at 0x24000000

MAC:   02:80:AD:24:31:E8

I2C:   ready

Hit any key to stop autoboot:  0

bfin>

bfin> print

baudrate=57600

loads_echo=1

ethaddr=02:80:ad:24:31:e8

autoload=no

rootpath=/romfs

hostname=BF548

ramargs=setenv bootargs root=/dev/mtdblock0 rw

nfsargs=setenv bootargs root=/dev/nfs rw nfsroot=$(serverip):$(rootpath)

addip=setenv bootargs $(bootargs) ip=$(ipaddr):$(serverip):$(gatewayip):$(netmask):$(hostname):eth0:off

ramboot=tftpboot 0x1000000 linux;run ramargs;run addip;bootelf

nfsboot=tftpboot 0x1000000 linux;run nfsargs;run addip;bootelf

flashboot=bootm 0x20100000

update=tftpboot 0x1000000 u-boot.ldr;eeprom write 0x1000000 0x0 $(filesize)

date_tested=Tue Nov 6 01:54:26 CST 2007

filesize=32398

fileaddr=1000000

mmcargs=setenv bootargs root=B301 rw

mmcboot=tftpboot 0x1000000 vmlinux; run mmcargs; run addip; bootelf

netmask=255.255.255.0

tftp_load=tftpboot 0x1000000 linux;run bootargs;run addip;bootelf

gatewayip=192.168.0.1

ipaddr=10.100.4.50

serverip=10.100.4.174

bootdelay=5

bootargs=root=/dev/mtdblock0 rw earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF0,57600 ip=10.100.4.50

bootcmd=run tftp_boot

tftp_boot=tftp 0x2000000 linux;boote

stdin=serial

stdout=serial

stderr=serial

 

Environment size: 1102/8188 bytes

bfin> mtest

Pattern 00000000  Writing...  Reading...

Mem error @ 0x03EFBA8C: found 03FA041A, expected 00F7EEA3

 

Mem error @ 0x03EFBA90: found 45453746, expected 00F7EEA4

 

Mem error @ 0x03EFBA94: found 000A3441, expected 00F7EEA5

 

Mem error @ 0x03EFBA98: found 00000000, expected 00F7EEA6

 

Mem error @ 0x03EFBA9C: found 00000001, expected 00F7EEA7

 

Mem error @ 0x03EFBAAC: found 03FA00B2, expected 00F7EEAB

 

Mem error @ 0x03EFBAB0: found 00000032, expected 00F7EEAC

 

Mem error @ 0x03EFBAB4: found 00000026, expected 00F7EEAD

                                                                                                                                                           ..

 

Follow-ups

 

--- Mike Frysinger                                           2008-06-19 00:26:57

ive already fixed this in trunk ... the default mtest clobbers the stack on

bf548-ezkit

 

--- Mike Frysinger                                           2008-06-26 00:49:28

which means this is fixed in the 2008R1.5 branch ... wont bother for 2008R1

branch

 

--- Mingquan Pan                                             2008-06-26 06:46:00

Yes,fixed. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes