[#3892] 08r1 branch head uboot has no boote command on bf537

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

[#3892] 08r1 branch head uboot has no boote command on bf537

Submitted By: Mingquan Pan

Open Date

2008-02-13 02:24:46     Close Date

2008-02-13 20:03:46

Priority:

Medium     Assignee:

Mike Frysinger

Category:

N/A     Fixed In Release:

N/A

Found In Release:

N/A     Status:

Closed

Board:

N/A     Processor:

N/A

Silicon Revision:

    Resolution:

Fixed

Is the bug repeatable?:

N/A     

Summary: 08r1 branch head uboot has no boote command on bf537

Details:

 

08r1 branch head uboot has no boote command on bf537.

 

U-Boot 1.1.6-svn1145 (ADI-2008R1) (Feb 13 2008 - 17:28:28)

 

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   00:00:11:22:33:22

I2C:   ready

Hit any key to stop autoboot:  0

bfin>

bfin> boote

Unknown command 'boote' - try 'help'

bfin>

bfin> help

?       - alias for 'help'

autoscr - run script from memory

base    - print or set address offset

bdinfo  - print Board Info structure

boot    - boot default, i.e., run 'bootcmd'

bootd   - boot default, i.e., run 'bootcmd'

bootldr - boot ldr image from memory

bootm   - boot application image from memory

bootp   - boot image via network using BootP/TFTP protocol

cmp     - memory compare

coninfo - print console devices and information

cp      - memory copy

cplbinfo- display current CPLB tables

crc32   - checksum calculation

echo    - echo args to console

erase   - erase FLASH memory

flinfo  - print FLASH memory information

go      - start application at address 'addr'

help    - print online help

iminfo  - print header information for application image

imls    - list all images found in flash

itest   - return true/false on integer compare

loadb   - load binary file over serial line (kermit mode)

loads   - load S-Record file over serial line

loady   - load binary file over serial line (ymodem mode)

loop    - infinite loop on address range

md      - memory display

mm      - memory modify (auto-incrementing)

mtest   - simple RAM test

mw      - memory write (fill)

nfs     - boot image via network using NFS protocol

nm      - memory modify (constant address)

printenv- print environment variables

protect - enable or disable FLASH write protection

rarpboot- boot image via network using RARP/TFTP protocol

reset   - Perform RESET of the CPU

run     - run commands in an environment variable

saveenv - save environment variables to persistent storage

setenv  - set environment variables

sleep   - delay execution for some time

tftpboot- boot image via network using TFTP protocol

version - print monitor version

 

while on bf533 board, this command works right.

 

Follow-ups

 

--- Mike Frysinger                                           2008-02-13 15:30:20

looks like the branch had a few more BFIN_BOOT_MODE than trunk in the

bf537-stamp config file so they werent all converted to CONFIG_BFIN_BOOT_MODE

 

should be fixed now

 

--- Mingquan Pan                                             2008-02-13 22:12:42

Yes,close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes